function bf = setupPhaser(rx,phaserURI,fc) % Copyright 2023 The MathWorks, Inc. % Configure phaser bf = adi.Phaser; bf.uri = phaserURI; bf.SkipInit = true; % Bypass writing all initial attributes to speed things up bf(); bf.ElementSpacing = 0.014; % Put device in Rx mode bf.TxRxSwitchControl = {'spi','spi'}; bf.Mode(:) = {'Disabled'}; bf.BeamMemEnable(:) = false; bf.BiasMemEnable(:) = false; bf.PolState(:) = false; bf.PolSwitchEnable(:) = false; bf.TRSwitchEnable(:) = true; bf.ExternalTRPolarity(:) = true; bf.RxVGAEnable(:) = true; bf.RxVMEnable(:) = true; %? bf.RxLNABiasCurrent(:) = 8; bf.RxVGABiasCurrentVM(:) = 22; % Self bias LNAs bf.LNABiasOutEnable(:) = false; % Fire them up bf.RxPowerDown(:) = false; bf.Mode(:) = {'Rx'}; % Set up PLL bf.Frequency = (fc + rx.CenterFrequency) / 4; BW = 500e6 / 4; num_steps = 1000; bf.FrequencyDeviationRange = BW; % frequency deviation range in H1. This is the total freq deviation of the complete freq ramp bf.FrequencyDeviationStep = int16(BW / num_steps); % frequency deviation step in Hz. This is fDEV, in Hz. Can be positive or negative bf.RampMode = "disabled"; bf.DelayStartWord = 4095; bf.DelayClockSource = "PFD"; bf.DelayStartEnable = false; % delay start bf.RampDelayEnable = false; % delay between ramps. bf.TriggerDelayEnable = false; % triangle delay bf.SingleFullTriangleEnable = false; % full triangle enable/disable -- this is used with the single_ramp_burst mode bf.TriggerEnable = false; % start a ramp with TXdata % Flatten phaser phase/gain bf.RxGain(:) = 127; bf.RxAttn(:) = 0; bf.RxPhase(:) = 0; bf.RxLNAEnable(:) = true; bf.LatchRxSettings(); end