function txFrequency = findTxFrequency() % Setup: % % Place the HB100 in front of the Phaser - 0 degree azimuth. % % Notes: % % The frequency of the phaser is swept between 10 and 10.5 GHz. The peak % frequency is measured. This is assumed to be the frequency of the HB100. % % Copyright 2023 The MathWorks, Inc. % Setup the frequencies to scan. f_start = 10.e9; f_stop = 10.5e9; f_step = 5e6; fvec = f_start : f_step : f_stop; % Setup the antenna, setting the frequency to f_start. [rx,bf,~] = setupAntenna(f_start); % Setup variables for capturing scan amplitude and frequency. full_ampl = []; full_freqs = []; N = rx.SamplesPerFrame; % Loop through the frequency vector and save receive data at each center % frequency. for centerfrequency = fvec % The LO is set to 4x the Frequency setting. %%% VI : Where is this ? I see line 31 in setupPhaser looking similar %%% to this bf.Frequency = (centerfrequency + rx.CenterFrequency)/4; rx(); % Capture the data, sum the channels, and convert to the frequency domain data = rx(); data = sum(data,2); famplitude = mag2db(1/N * fftshift(abs(fft(data)))); full_ampl = [full_ampl, famplitude]; % Get the frequency span for this data sample df = rx.SamplingRate/N; band = (-rx.SamplingRate/2 : df : rx.SamplingRate/2 - df); freqspan = centerfrequency-band; full_freqs = [full_freqs, freqspan']; end % Get the max amplitude for each measurement [maxamplitudes,maxidxs] = max(full_ampl); % Get the max amplitude in the whole dataset [~,maxframeidx] = max(maxamplitudes); maxdatapointidx = maxidxs(maxframeidx); txFrequency = full_freqs(maxdatapointidx,maxframeidx); ax = axes(figure); plot(ax,full_freqs/1e9,full_ampl); xlabel('Frequency (GHz)'); ylabel('Amplitude (dB)'); title(ax,['HB100 Frequency = ' num2str(txFrequency/1e9) 'GHz']); end