ADRV9002 (Jupiter) Plugin
Description
The ADRV9002 (Jupiter) plugin provides a comprehensive interface for controlling and configuring the ADRV9002 dual-channel RF transceiver. This plugin enables users to manage both receive and transmit signal paths, configure device settings, and control FPGA-based signal generation features. The ADRV9002 is a dual-channel RF transceiver designed for software-defined radio applications with wide bandwidth and high performance.
The plugin is organized into four main sections providing complete control over the device functionality:
Device Global Settings - System-wide configuration and status monitoring
Receive Chain - RX channel configuration and signal path control
Transmit Chain - TX channel configuration and signal path control
Profile Generator - Integrated tools for creating and managing device profiles
Compatible Devices
The ADRV9002 plugin is compatible with:
ADRV9002 dual-channel RF transceiver platforms
Systems implementing the ADRV9002 IIO driver interface
Hardware platforms with ADRV9002 integrated designs
Note
This plugin requires a compatible IIO context with ADRV9002 device support. Ensure that the appropriate device drivers are installed and the hardware is properly connected.
Device Global Settings
The Device Global Settings section provides system-wide controls and monitoring capabilities:
- Profile Configuration
Allows loading of profile configurations from external files. Profiles define the operational parameters including sampling rates, bandwidths, and signal path configurations.
Load Profile: Browse and select profile configuration files
Profile Status: Displays current profile information
For detailed information about profiles, see the ADRV9002 Driver Documentation.
Note
The plugin includes an integrated Profile Generator tab for creating profiles. This feature requires the external libadrv9002-iio library to be installed.
- Temperature Monitoring
Reports the current device temperature for thermal monitoring and protection.
Temperature Display: Real-time device temperature in degrees Celsius
Temperature Status: Indicates normal operation or thermal warnings
- Device Information
Displays device identification and version information:
Device Driver Version: Current driver version information
Hardware Revision: Device hardware revision details
Firmware Version: Loaded firmware version
Receive Chain Configuration
The Receive Chain section provides comprehensive control over the RX signal path for both channels:
Signal Path Parameters
- RF Bandwidth (MHz)
Displays the Primary Signal Bandwidth of the currently loaded profile. This parameter defines the usable signal bandwidth for the receive path.
- Sampling Rate (MSPS)
Shows the RX Sample Rate configured in the current profile. This determines the digital sampling frequency for received signals.
Gain Control Settings
- Gain Control Mode
Selects the gain control mechanism:
SPI: Manual gain control via software interface
PIN: Hardware pin-controlled gain adjustment
Automatic: Automatic gain control (AGC) mode
- Hardware Gain (dB)
Controls the RX gain when in SPI or PIN mode. This setting adjusts the analog gain in the receive signal path.
Signal Monitoring
- RSSI (dB)
Displays the Received Signal Strength Indicator, providing real-time measurement of input signal level.
- Decimated Power (dB)
Shows the decimated power measurement, useful for signal analysis and monitoring.
Frequency Control
- NCO (Hz)
Controls the Numerically Controlled Oscillator for frequency offset correction. This setting is only available if the loaded profile supports NCO correction.
- Local Oscillator (MHz)
Controls the carrier frequency for the receive chain. This sets the center frequency for signal reception.
Channel Control
- Enable
While off disables the transmit channel, stopping signal transmission and reducing power consumption.
- Dynamic ADC Switch
Enables dynamic ADC switching functionality for optimized power management and performance.
- ENSM (Enable State Machine)
Selects the operational mode for the Enable State Machine:
Calibrated: Normal operation with calibrations enabled
Primed: Standby mode ready for quick activation
RF Enabled: Full RF operation mode
- Port Enable
Configures how the port can be enabled:
SPI: Software-controlled port enable
PIN: Hardware pin-controlled port enable
Digital Signal Processing
- Digital Gain Control
Selects the digital gain control mode for fine-tuning signal levels in the digital domain.
- Interface Gain (dB)
Controls the Slicer block gain for digital signal processing optimization.
- Tracking Calibrations
Enable/disable various tracking calibration algorithms:
Quadrature FIC: Quadrature frequency image correction
BBDC Rejection: Baseband DC offset rejection
HD2: Second harmonic distortion correction
AGC: Automatic gain control calibration
Quadrature Poly: Quadrature polynomial correction
RSSI: RSSI calibration
RDFC: Receive data formatting correction
Transmit Chain Configuration
The Transmit Chain section provides control over the TX signal path for both channels:
Signal Path Parameters
- RF Bandwidth (MHz)
Displays the Primary Signal Bandwidth for the transmit path as defined in the current profile.
- Sampling Rate (MSPS)
Shows the TX Sample Rate configured in the current profile, determining the digital sampling frequency for transmitted signals.
Power Control
- Attenuation (dB)
Controls the TX output power attenuation. Higher values reduce output power.
- Attenuation Control Mode
Selects the attenuation control mechanism:
SPI: Software-controlled attenuation
PIN: Hardware pin-controlled attenuation
Bypass: Bypass attenuation control
Channel Control
- ENSM (Enable State Machine)
Configures the transmit channel operational mode similar to the receive chain.
- Port Enable
Selects port enable control method (SPI or PIN) for the transmit channel.
- Enable
While off disables the transmit channel, stopping signal transmission and reducing power consumption.
Frequency Control
- NCO (Hz)
Controls frequency offset correction for the transmit path when supported by the loaded profile.
- Local Oscillator (MHz)
Sets the carrier frequency for signal transmission.
- Tracking Calibrations
Enable/disable transmit-specific calibration algorithms:
Quadrature: Quadrature correction for TX path
PA Correction: Power amplifier linearity correction
LO Leakage: Local oscillator leakage correction
Close Loop Gain: Closed-loop gain calibration
Loopback Delay: Loopback delay calibration
Profile Generator
The ADRV9002 plugin includes an integrated Profile Generator tab that provides a graphical interface for creating and managing ADRV9002 device profiles. This functionality requires an external dependency to be installed.
Warning
The Profile Generator functionality requires the libadrv9002-iio library to be installed. If this external tool is missing, the Profile Generator functionality will be disabled. The library can be obtained from: https://developer.analog.com/docs/libadrv9002-iio
Profile Generator Interface
The Profile Generator tab is accessible through the main plugin interface and provides the following sections:
- Profile Generator CLI Detection
Displays the status of the external profile generator tool:
- Profile Actions
Preset Dropdown: Select from predefined profile templates (“LTE” or “Live Device”)
Refresh Button: Reload available presets and update the interface
Save Stream to file: Export the generated stream configuration to a file
Save Profile to file: Export the profile configuration to a file
Load to device: Apply the current profile configuration to the connected ADRV9002 device
Radio Configuration
SSI Interface: Show the Serial Synchronous Interface type (LVDS/CMOS)
Duplex mode: Choose between TDD (Time Division Duplex) and FDD (Frequency Division Duplex)
- Channel Configuration
The interface provides separate configuration sections for each channel:
- RX Channels (RX 1 / RX 2)
For each receive channel, the following options are available:
Enabled: Checkbox to enable/disable the RX channel
Frequency Offset Correction: Enable frequency offset correction capability
Bandwidth (Hz): Set the channel bandwidth (e.g., 38000000)
Interface Sample Rate (Hz): Configure the sample rate (e.g., 61440000)
RX RF Input: Select the RF input path (RxA/RxB)
- TX Channels (TX 1 / TX 2)
For each transmit channel, the following options are available:
Enabled: Checkbox to enable/disable the TX channel
Frequency Offset Correction: Enable frequency offset correction capability
Bandwidth (Hz): Set the channel bandwidth (e.g., 38000000)
Interface Sample Rate (Hz): Configure the sample rate (e.g., 61440000)
- ORX Configuration
Observation Receiver channels for monitoring and calibration
- Debug Information
Displays the JSON configuration being generated:
Configuration Preview: Shows the profile configuration in JSON format
Real-time Updates: Updates automatically as parameters are changed
Technical Details: Displays low-level configuration parameters
External Tool Dependency
The Profile Generator relies on the libadrv9002-iio library:
Installation Required: Must be installed separately from Scopy
Version Compatibility: Different versions support different ADRV9002 API versions
CLI Integration: Scopy interfaces with the command-line tool provided by the library
Automatic Detection: Scopy automatically detects if the tool is available
Supported API Versions
The external tool supports multiple ADRV9002 API versions:
v68.8.1 (v0.24): Supported in libadrv9002-iio v0.1.0 and v0.2.0
v68.10.1 (v0.25): Supported in libadrv9002-iio v0.2.0 and later
Note
If the Profile Generator tab appears grayed out or disabled, check that the libadrv9002-iio library is properly installed and accessible in the system PATH.
Note
Profile configurations are device-specific and must match the connected ADRV9002 hardware capabilities. Invalid configurations will be rejected when loaded to the device.