pyadi-jif MCP Server

The pyadi-jif Model Context Protocol (MCP) server provides a programmatic interface for interacting with pyadi-jif functionalities, including querying JESD modes and performing system-level solving. This server leverages the fastmcp library to expose its capabilities as discoverable tools, making it accessible to AI assistants and other automated systems.

Installation

Install pyadi-jif with the mcp optional extras:

pip install "pyadi-jif[mcp]"

Starting the Server

stdio (default — for Claude Desktop and local tools)

jifmcp

HTTP transport

jifmcp --transport http --port 8000

Claude Desktop Integration

Add the following snippet to your claude_desktop_config.json to connect pyadi-jif to Claude Desktop:

{
  "mcpServers": {
    "pyadi-jif": {
      "command": "jifmcp",
      "args": []
    }
  }
}

The config file is located at:

  • macOS: ~/Library/Application Support/Claude/claude_desktop_config.json

  • Windows: %APPDATA%\Claude\claude_desktop_config.json

  • Linux: ~/.config/Claude/claude_desktop_config.json

Restart Claude Desktop after saving the file. The pyadi-jif tools will appear in the tools panel.

Available Tools

list_components

Lists all available components of a given type.

list_components(component_type: str) -> dict

Parameter

Type

Description

component_type

str

One of "converter", "clock", or "fpga".

Returns a dict with a "components" key containing a list of component name strings.


get_component_info

Retrieves the docstring, constructor signature, and public properties of a specific component.

get_component_info(component_type: str, component_name: str) -> dict

Parameter

Type

Description

component_type

str

One of "converter", "clock", or "fpga".

component_name

str

Component name as returned by list_components (e.g. "AD9081_RX").

Returns a dict with keys name, docstring, constructor_signature, and properties.


query_jesd_modes

Queries the available JESD modes for a converter component, optionally filtered by JESD parameters.

query_jesd_modes(component_name: str, jesd_params_json: str = "{}") -> dict

Parameter

Type

Description

component_name

str

Converter name (e.g. "AD9081_RX", "ADRV9009_TX").

jesd_params_json

str

JSON string of JESD filter parameters (e.g. '{"M": 4, "L": 8, "K": 32}'). Default: "{}" (all modes).

Returns a dict with keys component, jesd_modes (list), and query_params.


solve_system

Performs system-level clock and JESD solving based on a JSON configuration.

solve_system(system_config_json: str) -> dict

Parameter

Type

Description

system_config_json

str

JSON string describing the system. See schema below.

Returns a dict with keys status ("solved"), solution, and config on success, or error on failure.

system_config_json Schema

{
  "conv": "AD9081_RX",
  "clk": "HMC7044",
  "fpga": "XILINX_BF",
  "vcxo": {
    "type": "fixed",
    "value": 100000000
  },
  "solver": "CPLEX",
  "converter_properties": {
    "sample_clock": 1000000000,
    "jesd_class": "jesd204c",
    "M": 4,
    "L": 8,
    "F": 1
  },
  "clock_properties": {
    "jesd_class": "jesd204c"
  },
  "fpga_properties": {},
  "pll_configurations": [
    {
      "type": "inline",
      "name": "ADF4371",
      "vcxo": { "type": "fixed", "value": 122880000 },
      "target_component": "converter",
      "pll_properties": {
        "r_divider": 1,
        "n_divider": 20
      }
    }
  ],
  "constraints": {}
}

Field reference:

Field

Required

Description

conv

yes

Converter name (e.g. "AD9081_RX").

clk

yes

Clock chip name (e.g. "HMC7044").

fpga

yes

FPGA name (e.g. "XILINX_BF").

vcxo

no

VCXO config. Default: {"type": "fixed", "value": 100000000}.

vcxo.type

—

"fixed" (requires value), "range" (requires start, stop, step), or "arb_source" (requires frequency, count).

solver

no

Solver to use. Default: "CPLEX". Also supports "GEKKO".

converter_properties

no

Attributes to set on the converter instance.

clock_properties

no

Attributes to set on the clock instance.

fpga_properties

no

Attributes to set on the FPGA instance.

pll_configurations

no

List of inline or sysref PLL configs. Each entry has type, name, vcxo, target_component, and pll_properties.

constraints

no

Output clock constraints dict passed to sys.solve().

Python Client Example

import asyncio
import json
from fastmcp import Client
from adijif.mcp_server import create_mcp_server

async def main():
    server = create_mcp_server()
    async with Client(server) as client:
        # List available converters
        result = await client.call_tool("list_components", {"component_type": "converter"})
        print("Converters:", result.data["components"])

        # Query JESD modes for AD9081_RX filtered by M=4, L=8
        result = await client.call_tool(
            "query_jesd_modes",
            {
                "component_name": "AD9081_RX",
                "jesd_params_json": json.dumps({"M": 4, "L": 8}),
            },
        )
        print("JESD modes:", result.data["jesd_modes"])

        # Solve a system
        system_config = {
            "conv": "AD9081_RX",
            "clk": "HMC7044",
            "fpga": "XILINX_BF",
            "vcxo": {"type": "fixed", "value": 100000000},
            "solver": "CPLEX",
            "converter_properties": {
                "sample_clock": 1000000000,
                "jesd_class": "jesd204c",
                "M": 4,
                "L": 8,
                "F": 1,
            },
            "clock_properties": {"jesd_class": "jesd204c"},
        }
        result = await client.call_tool(
            "solve_system", {"system_config_json": json.dumps(system_config)}
        )
        if "error" in result.data:
            print("Error:", result.data["error"])
        else:
            print("Solution:", result.data["solution"])

asyncio.run(main())