Debugging with Xilinx Vitis IDE

Important

The make sdkopen command automatically detects your Vitis version and launches the appropriate IDE:

  • Vitis 2023.1 and older: Classic Eclipse-based IDE

  • Vitis 2023.2 - 2024.x: Classic Eclipse-based IDE (using -classic flag for stability)

  • Vitis 2025.1 and newer: Unified IDE (VSCode-based)

Why Classic Mode for Vitis 2023.2-2024.x?

Vitis 2023.2 introduced the Unified IDE, but the User Managed Mode (required for makefile-based projects) has incomplete debug configuration support. The classic Eclipse mode provides a mature, fully-functional debugging experience for these versions.

This guide covers debugging workflows for all Vitis versions:

  • Vitis 2023.2-2024.x: Classic Eclipse IDE workflow (Step 3A)

  • Vitis 2025.1+: Unified IDE workflow (Step 3B)

Prerequisites

  • Vitis installed (any version)

  • Hardware design file (.xsa) in project directory

  • JTAG and UART cables connected to target board

Note

After the IDE opens, proceed to the appropriate section based on your Vitis version:

  • Vitis 2023.2-2024.x: Continue to Step 3A (Classic Eclipse workflow)

  • Vitis 2025.1+: Continue to Step 3B (Unified IDE workflow)

WSL2 Users: One-Time xsdb Fix

Important

On WSL2, xsdb crashes with "Segmentation fault" due to rlwrap incompatibility. Apply this fix once per machine.

If you've already applied this fix previously, skip this step.

Manual Installation

Note

The paths shown use the default Vitis installation directory. If you installed Vitis to a different location, adjust the paths accordingly.

cd /path/to/no-OS

# Backup original
# Replace /xilinx/2025.1 with your Vitis installation path
sudo cp /xilinx/2025.1/Vitis/bin/xsdb /xilinx/2025.1/Vitis/bin/xsdb.original

# Install fixed version
sudo cp tools/scripts/platform/xilinx/xsdb-nowrap /xilinx/2025.1/Vitis/bin/xsdb
sudo chmod +x /xilinx/2025.1/Vitis/bin/xsdb

Per-Project Setup (First Time Only)

Step 1: Build Project

source /xilinx/2025.1/Vitis/settings64.sh
cd /path/to/no-OS/projects/your_project
make

What happens:

  • First build automatically runs make project (generates BSP and FSBL)

  • Compiles application

  • Creates build/your_project.elf

Tip

You do NOT need to run make project manually - make calls it automatically when needed!

Building in Debug Mode

To enable debugging with proper compiler flags:

make DEBUG=1

What this does:

  • Disables optimization: -O0 (so breakpoints work correctly)

  • Adds full debug symbols: -g3

  • Remaps debug paths: -fdebug-prefix-map (so debugger finds source files)

For production/release builds, simply use make without DEBUG=1 to get optimized code.

Tip

You can set DEBUG = 1 in your project Makefile to always build in debug mode for that project.

Step 2: Open Vitis IDE

make sdkopen

What happens:

  • The command automatically detects your Vitis version

  • For Vitis 2025.1+: Unified IDE opens at project root

    • First time only: You'll see "Update Workspace" dialog - Click "Update" to initialize

    • Workspace metadata initialized (after clicking Update)

    • _ide/ directory created with workspace configuration

    • Debug configuration automatically generated (_ide/launch.json)

    • Bitstream and initialization files extracted from XSA

  • For Vitis 2023.2-2024.x: Classic Eclipse IDE opens

    • Workspace opens at build/ directory

    • Standard Eclipse workspace with .metadata/ directory

    • Manual debug configuration required (see Step 3A)

Choose Your Workflow

The next steps depend on your Vitis version:

  • Vitis 2023.2-2024.x users: Continue to Step 3A (manual debug configuration)

  • Vitis 2025.1+ users: Skip to Step 3B (automated)

Step 3A: Create Debug Configuration (Classic Eclipse - Vitis 2023.2-2024.x)

Note

This section is for Vitis 2023.2-2024.x users only. If you're using Vitis 2025.1+, skip to Step 3B below.

A. Open Debug Configurations Dialog

In the Vitis IDE menu bar:

  • Go to Run → Debug Configurations...

  • Or click the Debug toolbar button dropdown → Debug Configurations...

The "Debug Configurations" dialog will open.

B. Create New Configuration

  1. In the left panel, expand "Single Application Debug"

  2. Click the "New Configuration" button (first icon in the toolbar - looks like a document with a star/plus)

  3. A new configuration will be created (e.g., Debugger_-Default)

  4. You can rename it if desired (e.g., adrv904x-debug)

C. Configure Main Tab

The "Main" tab should be selected by default.

Debug Type:

  • Select "Standalone Application Debug" from the dropdown

  • (Not "Attach to running target" - we want to reset and program the system)

Connection:

  • Leave as "Local" (debugging via local JTAG connection)

D. Configure Target Setup Tab

Click the "Target Setup" tab at the top.

Hardware Platform:

  • Should auto-populate with the path to your .xsa file

  • If empty, click "Browse..." and select system_top.xsa from your project root

Bitstream File:

  • Auto-populated from the XSA file

  • Path will be similar to: .../projects/your_project/system_top.bit

FSBL Configuration (ZynqMP/Zynq-7000 only):

Check these boxes:

  • ☑ Use FSBL flow for initialization

  • ☑ Reset entire system

  • ☑ Program FPGA

  • ☑ Initialize using FSBL

FSBL File:

Browse to or enter the FSBL path:

build/tmp/output/hw0/export/hw0/sw/hw0/boot/fsbl.elf

Note

For MicroBlaze: Uncheck "Use FSBL flow for initialization" - MicroBlaze doesn't use FSBL

Summary Panel:

After configuration, the Summary panel on the right shows the debug sequence:

  1. Reset system and clear FPGA

  2. Program FPGA with bitstream

  3. Initialize PS using FSBL

  4. Load application and suspend processors

E. Configure Application Tab

Click the "Application" tab at the top.

Processor Selection:

The IDE shows a table with available processors. Check the box next to your target processor:

  • ZynqMP: psu_cortexa53_0 (or psu_cortexr5_0 for R5)

  • Zynq-7000: ps7_cortexa9_0

  • MicroBlaze: microblaze_0

  • Versal: psv_cortexa72_0

Project and Application:

The IDE typically auto-populates these fields:

  • Project: Should show your project name (e.g., adrv904x)

  • Application: Should point to your ELF file:

    build/your_project.elf
    

Tip

If the Application field is empty, click "Search..." and browse to build/your_project.elf

Stop at 'main':

  • Check this box to have the debugger stop at the main() function (recommended)

F. Save and Apply

  1. Click "Apply" to save the configuration

  2. Click "Debug" to start debugging immediately, or "Close" to save for later

The configuration is now saved and ready to use!

Step 3B: Automatic Debug Configuration (Unified IDE - Vitis 2025.1+)

Note

This section is for Vitis 2025.1+ users only. If you're using Vitis 2023.2-2024.x, use Step 3A above instead.

Important

For optimal debugging experience, always build with make DEBUG=1 before debugging. This ensures proper optimization settings (-O0) and correct source path mapping.

Debug Configuration

When you run make sdkopen with Vitis 2025.1+, the build system automatically:

  1. Extracts hardware files from the XSA:

    • Bitstream (_ide/system_top/system_top.bit)

    • Initialization script (psu_init.tcl or ps_init.tcl)

  2. Generates debug configuration (_ide/launch.json) with:

    • Correct architecture-specific settings (ZynqMP, Zynq-7000, MicroBlaze, Versal)

    • Hardware platform path (XSA file)

    • FSBL configuration (if applicable)

    • Application ELF path

    • Target processor

What this means: No manual configuration needed! The debug configuration is ready to use.

Verify Configuration (Optional)

If you want to verify or customize the generated configuration:

  1. In Vitis Explorer, expand _ide folder

  2. Open launch.json to view the configuration

  3. You'll see a configuration named <project_name>_app_hw_1

The configuration is automatically regenerated each time you run make sdkopen.

Debugging Your Project

Hardware Setup

  • Connect JTAG cable to your board

  • Connect UART cable (for console output)

  • Power on the board

Start Debugging

Prerequisites:

  1. Make sure you've built your project: make (in terminal)

  2. Hardware connected (JTAG and UART cables, board powered on)

Classic Eclipse IDE (Vitis 2023.2-2024.x):

  1. Go to Run → Debug Configurations...

  2. Select your debug configuration (e.g., "adrv904x-debug")

  3. Click "Debug" button

  4. The Debug perspective will open automatically

Unified IDE (Vitis 2025.1+):

  1. Click FLOW panel (left side) → Click "Debug"

  2. The debug session will start

Note

The Start Debugging (F5) button in the Debug panel does not currently work for Vitis 2025.1. You must use the FLOW → Debug button to start debugging sessions.

What happens (both versions):

  • Vitis connects to board via JTAG

  • Programs FPGA with bitstream

  • Runs FSBL to initialize processor (ZynqMP/Zynq only)

  • Loads your application ELF

  • Stops at entry point (usually main()) - ready to debug!

Debug Features (both versions):

  • Set breakpoints (click left margin in code)

  • Step through code (F5=Step Into, F6=Step Over, F7=Step Return, F8=Resume)

  • Inspect variables, registers, call stack

  • Watch expressions

  • View memory and disassembly

Daily Development Workflow

After initial setup:

# 1. Edit code

# 2. Build with debug symbols (recommended for debugging)
make clean
make DEBUG=1

# 3. Open Vitis and debug
make sdkopen
# Click FLOW → Debug → Debugging starts!

Tip

For production builds (no debugging), use make without DEBUG=1 to get optimized code.

Architecture-Specific Notes

ZynqMP (Cortex-A53/R5)

  • Processor: psu_cortexa53_0 or psu_cortexr5_0

  • FSBL Required: Yes

  • FSBL Path: build/tmp/output/hw0/export/hw0/sw/hw0/boot/fsbl.elf

Zynq-7000 (Cortex-A9)

  • Processor: ps7_cortexa9_0

  • FSBL Required: Yes

  • FSBL Path: Same as ZynqMP

MicroBlaze

  • Processor: microblaze_0

  • FSBL Required: No (soft processor)

  • In launch.json: Set initWithFSBL: false

Versal (Cortex-A72)

  • Processor: psv_cortexa72_0

  • Uses PLM (Platform Loader Manager) instead of FSBL

Troubleshooting

"Segmentation fault" when debugging

Solution: Install xsdb WSL2 fix (see above)

Summary

One-time system setup:

  • Fix xsdb on WSL2 (if applicable)

Per-project setup:

  • Vitis 2023.2-2024.x (Classic Eclipse): Build → Open Vitis → Create debug configuration manually (Run → Debug Configurations) → Configure Application and Target Setup tabs → Apply

  • Vitis 2025.1+ (Unified IDE): Build → Open Vitis → Click "Update" → Debug configuration auto-generated!

Daily workflow:

# Vitis 2025.1+ (Unified IDE - AUTOMATED)
make clean && make DEBUG=1
make sdkopen
# Click FLOW → Debug → Debugging starts!

# Vitis 2023.2-2024.x (Classic Eclipse - Manual)
make clean && make DEBUG=1
make sdkopen
# Run → Debug Configurations → Select your config → Debug

Result: Streamlined debugging workflow for no-OS Xilinx projects across all Vitis versions.

Version-Specific Behavior

The make sdkopen command adapts to your Vitis version:

Vitis Version

IDE Type

Notes

2023.1 and older

Classic Eclipse

Manual debug configuration required

2023.2 - 2024.x

Classic Eclipse (via -classic flag)

Manual debug configuration required; Unified IDE User Managed Mode has incomplete debug support

2025.1 and newer

Unified IDE

Automatic debug configuration - launch.json auto-generated by build system

Additional Resources