AD9084/AD9088

The Apollo mixed signal front-end (MxFE®) is a highly integrated device with a 16-bit, 28/16 GSPS maximum sample rate, RF digital-to-analog converter (DAC) core, and 12-bit, 20/8 GSPS maximum sample rate, RF analog-to-digital converter (ADC) core. The AD9084/AD9088 supports eight transmit channels and eight receive channels. The AD9084/AD9088 is well suited for applications requiring both wideband ADCs and DACs to process signal(s) having wide instantaneous bandwidth. The device features a 48 lane, 28.1/32.51 Gbps JESD204C or 16/20 Gbps JESD204B data transceiver port, an on-chip clock multiplier, and a digital signal processing (DSP) capability targeted at either wideband or multi-band, direct to RF applications. The AD9084/AD9088 also features a bypass mode that allows the full bandwidth capability of the ADC and/or DAC cores to bypass the DSP datapaths. The device also features low latency loopback and frequency hopping modes targeted at phased array radar systems and electronic warfare applications.

Supported Devices

Evaluation Boards

Source Code

Is the driver in mainland? No.

The driver is divided into two groups: The API, and the Linux driver. The API is as an abstraction layer between the application and the hardware and is agnostic processor and operating system integration. The Linux Driver uses the API to connect the device to the Linux Kernel subsystems.

Note

The standalone sources for the API can be requested at AD9084 main page.

Linux Driver

API:

Interrelated Device Drivers

These are drivers that are connected to or is a dependency of ad9088.c.

Devicetree

The following example devicetrees are provided:

Profile

  • adi,device-profile-fw-name: Set the profile firmware to use.

See Device profile for more information.

Calibration

  • adi,device-calibration-data-name: Set the calibration data firmware file to load during driver probe. This enables automatic calibration restore from a previously saved calibration file, significantly reducing boot time.

If not present, the driver performs normal initialization with full calibration. See Calibration Data Management for more information.

Bring-up

  • adi,delayed-serdes-jrx-cal-en: Run SERDES calculation during the “link running” phase instead of the earlier “clocks enable” phase.

Format

  • adi,rx-real-channel-en: Disable complex Q/I samples for RX path.

  • adi,tx-real-channel-en: Disable complex Q/I samples for RX path.

In practice, doesn’t set the channel modifier, treating each channel as independent real channel. If not present, even number are I samples, and odd Q samples.

Trigger

  • adi,trigger-sync-en: Enable trigger synchronization.

  • adi,trig-req-gpio: Set the GPIO that trigger Enable trigger synchronization. If not provided, the SPI trigger will be used for trigger synchronization.

If the option is enabled and no trigger is provided, the synchronization will time out.

Multi-Chip Synchronization (MCS)

Topology

  • adi,side-b-use-seperate-tpl-en: Set side B to use own transport layer.

  • adi,standalone-enable: Allocate own IIO device to device. Top device always allocates IIO device through axiadc_converter, therefore has no effect on it.

  • adi,multidevice-instance-count: Define the total number of devices in the system on the main device. Only present if the subordinates uses adi,standalone-enable.

adi,multidevice-instance-count is a companion of the adi,standalone-enable attribute. For a topology of 4 devices, the main device has it set to 4, and the 3 subordinates contain the latter attribute.

SPI

  • adi,spi-3wire-enable: Use 3-wire SPI for SPI0.

HSCI

A few options are available to tune the HSCI interface.

  • adi,axi-hsci-connected: Sets the HSCI controller for the HSCI interface. If absent, only SPI is used to communicate with the device, considerably slower.

  • adi,hsci-auto-linkup-mode-en: Enable HSCI auto-linkup mode.

  • adi,hsci-disable-after-boot-en: Use SPI as the interface after initial device initialization.

GPIO

  • adi,gpio-exports: Expose a list of the 30s device GPIOs into a GPIO controller.

A more detailed usage is provided here.

Spectrum Sniffer

  • interrupt-names: fft_done_A" and fft_done_B for the spectrum sniffer interrupt signal for side a and b, respectively.

A more detailed usage is provided here.

Compile the driver

Configure kernel with make menuconfig (alternatively use make xconfig or make qconfig).

Linux Kernel Configuration
    Device Drivers  --->
        <*> JESD204 High-Speed Serial Interface Framework
    <*> Industrial I/O support --->
        --- Industrial I/O support
         -*-   Enable buffer support within IIO
         <*>     IIO callback buffer used for push in-kernel interfaces
         -*-     Industrial I/O DMA buffer infrastructure
         -*-     Industrial I/O DMA buffer integration with DMAEngine
         [*]       Enables I/O DMA buffer legacy MMAP support
         -*-     Industrial I/O HW buffering
         -*-     Industrial I/O buffering based on kfifo
         -*-     Industrial I/O triggered buffer support
         -*-   Enable IIO configuration via configfs
         -*-   Enable triggered sampling support
         <*>   Enable software IIO device support
         <*>   Enable software triggers support
         <*>   Enable triggered events support
         <*>   Analog Devices AXI ADXCVR PHY Support
         <*>   Generic AXI JESD204B configuration driver
         <*>   Analog Devices AXI JESD204B TX Support
         <*>   Analog Devices AXI JESD204B RX Support
         <*>   Analog Devices Generic IIO fake device driver
               Light sensors  --->
               Logic Analyzers  --->
         <*>   AXI AION Trigger support

           Analog to digital converters --->
         -*- Analog Devices High-Speed AXI ADC driver core
                 <*> Analog Devices AD9088 and similar Mixed Signal Front End (MxFE)

    Frequency Synthesizers DDS/PLL  --->
            Direct Digital Synthesis  --->
             <*> Analog Devices CoreFPGA AXI DDS driver
        Clock Generator/Distribution  --->
                     <*> Analog Devices HMC7044, HMC7043 Clock Jitter Attenuator with JESD204B
                     <*> Analog Devices ADF4030 10-Channel Precision Synchronizer

    <*>   JESD204 High-Speed Serial Interface Support  --->
        --- JESD204 High-Speed Serial Interface Support
        <*>   Analog Devices AXI ADXCVR PHY Support
        <*>   Analog Devices AXI JESD204B TX Support
        <*>   Analog Devices AXI JESD204B RX Support

Device profile

The device profiles can be generated with the profile generator tool that is part of the ACE Evaluation Software. Profile modifications can be done through pyadi-jif. In particular, the a Python Jupyter Notebook at examples/triton/triton_vcu118.ipynb guides you through the profile generation and modification, with sample files at the directory of the notebook. During runtime, some profile options are reconfigured, such as Fast Frequency Hopping.

With the device profile generated, compile into the kernel by adding it to the firmware folder and appending too the CONFIG_EXTRA_FIRMWARE kernel symbol. The firmware folder is set by the symbol CONFIG_EXTRA_FIRMWARE_DIR, if it is set to something else, add to that path instead. Then, update devicetree property adi,device-profile-fw-name.

You can have multiple profiles compiled into the kernel image by passing multiple profile paths, however only one set in the devicetree property. Consider using devicetree overlays to swapping profiles.

Usage

General IIO and driver conventions

Controlling the MxFE is done via the IIO sysfs interface. For convenience users can use Libiio and its various programming languages bindings.

The MxFE IIO device under /sys/bus/iio/devices/iio:deviceX features a set of channels and device attributes, which are explained here. Some basic, but important concepts are explained in the bullet list below:

  • Channels prefixed with **in_**voltageX apply to Receive (RX) ADC data paths.

  • Channels prefixed with **out**_voltageX apply to Transmit (TX) DAC data paths.

  • Each channel has a complex modifier in_voltageX_**i** and in_voltageX_**q** or out_voltageX_**i** and out_voltageX_**q**. Controlling a channel attribute for the i modified channel will simultaneously control the q modified channel and vice versa. So, writing/reading only needs to happen once, since they are mirrored. The complex IQ modifiers are only important for the data buffers, sine I & Q are individual data components.

  • IIO channels [in|out]_voltageX apply to the channelizer data paths (Fine DDC/DUC).

    • Each IIO channel has some [in|out]_voltageX_[i|q]_**channel**_[attributes]

    • In case the channelizer data paths (Fine DDC/DUC) are bypassed (decimation=1 or interpolation=1), the X still applies to a data path.

  • Each channelizer data path (FDDC, FDUC) connects at least to one Coarse DDC/DUC (CDDC/CDUC), which maps then to one or more ADCs/DACs depending on configuration. These are called main data paths and are controlled via the [in|out]_voltageX_[i|q]_**main**_[attributes] attributes.

    • Be aware, since multiple channels can map to the same main data path (CDDC/CDUC), changing a main attribute of one channel will also update same attribute of any other channel that maps to the same main data path (CDDC/CDUC).

    • The crossbar mapping between Fine and Coarse Digital Up/Down Converters, ADCs/DACs is defined in the device tree.

  • Device attributes (without **in_**voltageX``or ``**out_**voltageX prefix) apply to the entire device.

Driver testing

This device can be found under /sys/bus/iio/devices/

One way to check if the device and driver are present is using iio_info:

$
iio_info
    iio:device0: ad4052 (buffer capable)
            1 channels found:
                    voltage0:  (input, index: 0, format: le:s16/32>>0)
                    2 channel-specific attributes found:
                            attr  0: raw value: 12167
                            attr  1: sampling_frequency value: 1000000
            1 device-specific attributes found:
                            attr  0: waiting_for_supplier value: 0
            3 buffer-specific attributes found:
                            attr  0: data_available value: 0
                            attr  1: direction value: in
                            attr  2: length_align_bytes value: 8
            1 debug attributes found:
                            debug attr  0: direct_reg_access value: 0x10
            No trigger on this device

You can go to the device folder using:

$
cd $(grep -rw /sys/bus/iio/devices/*/name -e "ad9088" -l | xargs dirname)
/sys/bus/iio/devices/iio:device8$
ls -l
total 0
drwxr-xr-x 2 root root    0 Feb 11 15:17 buffer
drwxr-xr-x 2 root root    0 Feb 11 15:17 buffer0
-rw-r--r-- 1 root root 4096 Feb 11 15:17 calibration_data
--w------- 1 root root 4096 Feb 11 15:17 cfir_config
-r--r--r-- 1 root root 4096 Feb 11 15:17 dev
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_temp0_input
-r--r--r-- 1 root root 4096 Feb 11 15:17 in_temp0_label
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_cfir_en
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_cfir_profile_sel
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_channel_6db_digital_gain_en
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_channel_bmem_sample_delay
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_channel_nco_frequency
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_channel_nco_mixer_mode
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_channel_nco_phase
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_channel_nco_test_tone_scale
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_en
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_ffh_cnco_frequency
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_ffh_cnco_index
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_ffh_cnco_mode
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_ffh_cnco_select
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_ffh_fnco_frequency
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_ffh_fnco_index
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_ffh_fnco_mode
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_ffh_fnco_select
-r--r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_label
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_loopback
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_main_bmem_sample_delay
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_main_hb1_6db_digital_gain_en
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_main_nco_frequency
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_main_nco_mixer_mode
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_main_nco_phase
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_main_nco_test_tone_scale
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_main_tb1_6db_digital_gain_en
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_nyquist_zone
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_sampling_mode
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_i_test_mode
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_cfir_en
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_cfir_profile_sel
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_channel_6db_digital_gain_en
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_channel_bmem_sample_delay
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_channel_nco_frequency
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_channel_nco_mixer_mode
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_channel_nco_phase
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_channel_nco_test_tone_scale
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_en
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_ffh_cnco_frequency
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_ffh_cnco_index
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_ffh_cnco_mode
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_ffh_cnco_select
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_ffh_fnco_frequency
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_ffh_fnco_index
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_ffh_fnco_mode
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_ffh_fnco_select
-r--r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_label
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_loopback
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_main_bmem_sample_delay
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_main_hb1_6db_digital_gain_en
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_main_nco_frequency
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_main_nco_mixer_mode
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_main_nco_phase
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_main_nco_test_tone_scale
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_main_tb1_6db_digital_gain_en
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_nyquist_zone
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_sampling_mode
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage0_q_test_mode
...
-r--r--r-- 1 root root 4096 Feb 11 15:17 in_voltage_adc_frequency
-r--r--r-- 1 root root 4096 Feb 11 15:17 in_voltage_channel_nco_frequency_available
-r--r--r-- 1 root root 4096 Feb 11 15:17 in_voltage_channel_nco_mixer_mode_available
-r--r--r-- 1 root root 4096 Feb 11 15:17 in_voltage_loopback_available
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage_main_nco_frequency_available
-r--r--r-- 1 root root 4096 Feb 11 15:17 in_voltage_main_nco_mixer_mode_available
-r--r--r-- 1 root root 4096 Feb 11 15:17 in_voltage_nyquist_zone_available
-rw-r--r-- 1 root root 4096 Feb 11 15:17 in_voltage_sampling_frequency
-r--r--r-- 1 root root 4096 Feb 11 15:17 in_voltage_sampling_mode_available
-r--r--r-- 1 root root 4096 Feb 11 15:17 in_voltage_test_mode_available
-rw-r--r-- 1 root root 4096 Feb 11 15:17 jesd204_fsm_ctrl
-r--r--r-- 1 root root 4096 Feb 11 15:17 jesd204_fsm_error
-r--r--r-- 1 root root 4096 Feb 11 15:17 jesd204_fsm_paused
--w------- 1 root root 4096 Feb 11 15:17 jesd204_fsm_resume
-r--r--r-- 1 root root 4096 Feb 11 15:17 jesd204_fsm_state
-r--r--r-- 1 root root 4096 Feb 11 15:17 loopback1_blend_available
-rw-r--r-- 1 root root 4096 Feb 11 15:17 loopback1_blend_side_a
-rw-r--r-- 1 root root 4096 Feb 11 15:17 loopback1_blend_side_b
-r--r--r-- 1 root root 4096 Feb 11 15:17 name
lrwxrwxrwx 1 root root    0 Feb 11 15:17 of_node -> ../../../../../firmware/devicetree/base/fpga-axi@0/axi-ad9084-rx-hpc@a4a10000
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_i_cfir_en
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_i_cfir_profile_sel
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_i_channel_nco_frequency
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_i_channel_nco_mixer_mode
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_i_channel_nco_phase
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_i_channel_nco_test_tone_en
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_i_channel_nco_test_tone_scale
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_i_en
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_i_ffh_cnco_frequency
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_i_ffh_cnco_index
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_i_ffh_cnco_mode
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_i_ffh_cnco_select
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_i_ffh_fnco_frequency
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_i_ffh_fnco_index
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_i_ffh_fnco_mode
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_i_ffh_fnco_select
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_i_invsinc_en
-r--r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_i_label
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_i_main_nco_frequency
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_i_main_nco_mixer_mode
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_i_main_nco_phase
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_i_main_nco_test_tone_en
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_i_main_nco_test_tone_scale
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_q_cfir_en
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_q_cfir_profile_sel
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_q_channel_nco_frequency
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_q_channel_nco_mixer_mode
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_q_channel_nco_phase
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_q_channel_nco_test_tone_en
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_q_channel_nco_test_tone_scale
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_q_en
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_q_ffh_cnco_frequency
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_q_ffh_cnco_index
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_q_ffh_cnco_mode
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_q_ffh_cnco_select
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_q_ffh_fnco_frequency
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_q_ffh_fnco_index
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_q_ffh_fnco_mode
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_q_ffh_fnco_select
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_q_invsinc_en
-r--r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_q_label
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_q_main_nco_frequency
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_q_main_nco_mixer_mode
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_q_main_nco_phase
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_q_main_nco_test_tone_en
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage0_q_main_nco_test_tone_scale
...
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage_channel_nco_frequency_available
-r--r--r-- 1 root root 4096 Feb 11 15:17 out_voltage_channel_nco_mixer_mode_available
-r--r--r-- 1 root root 4096 Feb 11 15:17 out_voltage_dac_frequency
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage_main_nco_frequency_available
-r--r--r-- 1 root root 4096 Feb 11 15:17 out_voltage_main_nco_mixer_mode_available
-rw-r--r-- 1 root root 4096 Feb 11 15:17 out_voltage_sampling_frequency
--w------- 1 root root 4096 Feb 11 15:17 pfilt_config
drwxr-xr-x 2 root root    0 Feb 11 15:17 power
drwxr-xr-x 2 root root    0 Feb 11 15:17 scan_elements
lrwxrwxrwx 1 root root    0 Feb 11 15:17 subsystem -> ../../../../../bus/iio
-rw-r--r-- 1 root root 4096 Feb 11 15:17 sync_start_enable
-r--r--r-- 1 root root 4096 Feb 11 15:17 sync_start_enable_available
-rw-r--r-- 1 root root 4096 Feb 11 15:17 uevent
-r--r--r-- 1 root root 4096 Feb 11 15:17 waiting_for_supplier

Show channel name

The channel label contains the data path and it is shown with:

/sys/bus/iio/devices/iio:device8$
cat in_voltage2_q_label
Side-B:FDDC0->CDDC0->ADC0

ADC Rate

What: in_voltage_adc_frequency

Read only attribute which returns the RX ADC rate Hz.

/sys/bus/iio/devices/iio:device2$
cat in_voltage_adc_frequency
4000000000

RX Sample Rate

What: in_voltage_sampling_frequency

Read only attribute which returns the RX digital IQ base-band rate in Hz. This must not be confused with the ADC rate, which is (Main_decimation * Channel_decimation) time higher. Main_decimation, Channel_decimation are defined in the device tree.

in_voltage_sampling_frequency = \(in\_voltage\_adc\_frequency / (Main\_decimation * Channel\_decimation)\)

/sys/bus/iio/devices/iio:device2$
cat in_voltage_sampling_frequency
250000000

DAC Rate

What: out_voltage_dac_frequency

Read only attribute which returns the TX DAC rate Hz.

/sys/bus/iio/devices/iio:device2$
cat out_voltage_dac_frequency
20000000000

TX Sample Rate

What: out_voltage_sampling_frequency

Read only attribute which returns the TX digital IQ baseband rate in Hz. This must not be confused with the DAC rate, which is (Main_interpolation * Channel_interpolation) time higher. Main_interpolation, Channel_interpolation are defined in the device tree.

out_voltage_sampling_frequency = \(f_{DAC} / ({Main\_interpolation} * {Channel\_interpolation}\))

/sys/bus/iio/devices/iio:device2$
cat out_voltage_sampling_frequency
250000000

NCO Frequency Control

Main Data Path

What: [in|out]_voltageX_[i|q]_main_nco_frequency

Sets the main data path (CDDC/CDUC) NCO frequency (fCarrier) in Hz

  • out_voltageX_i_main_nco_frequency Range is: \(−f_{DAC}/2 ≤ f_{Carrier} < +f_{DAC}/2\)

  • in_voltageX_i_main_nco_frequency Range is: \(−f_{ADC}/2 ≤ f_{Carrier} < +f_{ADC}/2\)

/sys/bus/iio/devices/iio:device2$
echo 1000000000 > out_voltage0_i_main_nco_frequency
/sys/bus/iio/devices/iio:device2$
cat out_voltage0_i_main_nco_frequency
1000000000
/sys/bus/iio/devices/iio:device2$
echo 300000000 > in_voltage0_i_main_nco_frequency
/sys/bus/iio/devices/iio:device2$
cat in_voltage0_i_main_nco_frequency
300000000
Channel Data Path

What: [in|out]_voltageX_[i|q]_channel_nco_frequency

Sets the channel data path (FDDC/FDUC) NCO frequency (fCarrier) in Hz

out_voltageX_i_channel_nco_frequency range is:

\[−(f_{DAC}/Main\_interpolation)/2 ≤ f_{Carrier} < +(f_{DAC}/Main\_interpolation)/2\]

in_voltageX_i_channel_nco_frequency range is:

\[−(f_{ADC}/Main\_decimation)/2 ≤ f_{Carrier}< +(f_{ADC}/Main\_decimation)/2\]
/sys/bus/iio/devices/iio:device2$
echo 1000000000 > out_voltage0_i_channel_nco_frequency
/sys/bus/iio/devices/iio:device2$
cat out_voltage0_i_channel_nco_frequency
1000000000
/sys/bus/iio/devices/iio:device2$
echo 300000000 > out_voltage0_i_channel_nco_frequency
/sys/bus/iio/devices/iio:device2$
cat out_voltage0_i_channel_nco_frequency
300000000

NCO Phase Control

Main Data Path

What: [in|out]_voltageX_[i|q]_main_nco_phase

Sets the main data path (CDDC/CDUC) NCO phase offset in milli degrees

Range is: −180° ≤ Degrees Offset ≤ +180° (Values are in milli degrees.)

/sys/bus/iio/devices/iio:device2$
echo 66000 > out_voltage0_i_main_nco_phase
/sys/bus/iio/devices/iio:device2$
cat out_voltage0_i_main_nco_phase
66000
/sys/bus/iio/devices/iio:device2$
echo -42000 > in_voltage0_i_main_nco_phase
/sys/bus/iio/devices/iio:device2$
cat in_voltage0_i_main_nco_phase
-42000
Channel Data Path

What: [in|out]_voltageX_[i|q]_channel_nco_phase

Sets the channel data path (FDDC/FDUC) NCO phase offset in milli degrees

Range is: −180° ≤ Degrees Offset ≤ +180° (Values are in milli degrees.)

/sys/bus/iio/devices/iio:device2$
echo 13123 > out_voltage0_i_channel_nco_phase
/sys/bus/iio/devices/iio:device2$
cat out_voltage0_i_channel_nco_phase
13123

TX NCO Channel Digital Gain

What: out_voltageX_[i|q]_channel_nco_gain_scale

The input data into each channelizer stage can be rescaled prior to additional processing. This feature is useful in multiband applications to prevent digital clipping when the outputs of two or more channelizer stages are summed in the main datapath to produce a multiband band signal. The gain/scale is set via out_voltageX_[i|q]_channel_nco_gain_scale attribute.

Range is: \(0 ≤ Gain ≤ 1.999 (−∞ dB < dBGain ≤ +6.018 dB)\)

/sys/bus/iio/devices/iio:device2$
echo 0.707 > out_voltage0_i_channel_nco_gain_scale
/sys/bus/iio/devices/iio:device2$
cat out_voltage0_i_channel_nco_gain_scale
0.707

NCO Mixer Mode

What: [in|out]_voltageX_[i|q]_[main|channel]_nco_mixer_mode

Configures the NCO mixer mode for the main (CDDC/CDUC) or channel (FDDC/FDUC) data path. The mixer mode controls how the NCO frequency is applied to the signal.

Available modes can be read from the [in|out]_voltage_[main|channel]_nco_mixer_mode_available attribute:

  • var_IF: Variable IF mode (default)

  • zero_IF: Zero IF mode

  • fs/4_IF: Fs/4 IF mode

  • test_tone: Test tone mode

/sys/bus/iio/devices/iio:device8$
cat in_voltage_main_nco_mixer_mode_available
var_IF zero_IF fs/4_IF test_tone
/sys/bus/iio/devices/iio:device8$
echo var_IF > in_voltage0_i_main_nco_mixer_mode
/sys/bus/iio/devices/iio:device8$
cat in_voltage0_i_main_nco_mixer_mode
var_IF

NCO Test Tone

What: [in|out]_voltageX_[i|q]_[main|channel]_nco_test_tone_scale

Sets the NCO test tone scale for path testing. The test tone scale controls the amplitude of the internally generated test tone. The value is a floating point scale factor.

/sys/bus/iio/devices/iio:device8$
echo 0.5 > in_voltage0_i_main_nco_test_tone_scale
/sys/bus/iio/devices/iio:device8$
cat in_voltage0_i_main_nco_test_tone_scale
0.500000000

BMEM Sample Delay

What: in_voltageX_[i|q]_[main|channel]_bmem_sample_delay

Sets the buffer memory (BMEM) sample delay for the main (CDDC) or channel (FDDC) data path. This delay is used to align data paths when capturing samples to the buffer memory.

/sys/bus/iio/devices/iio:device8$
echo 10 > in_voltage0_i_main_bmem_sample_delay
/sys/bus/iio/devices/iio:device8$
cat in_voltage0_i_main_bmem_sample_delay
10

Sampling Mode

What: in_voltageX_[i|q]_sampling_mode

Configures the RX channel sampling mode. Available modes can be read from the in_voltage_sampling_mode_available attribute:

  • random: Random sampling mode (default)

  • sequential: Sequential sampling mode

/sys/bus/iio/devices/iio:device8$
cat in_voltage_sampling_mode_available
random sequential
/sys/bus/iio/devices/iio:device8$
echo random > in_voltage0_i_sampling_mode
/sys/bus/iio/devices/iio:device8$
cat in_voltage0_i_sampling_mode
random

Temperature Sensor

What: in_temp0_input, in_temp0_label

The AD9088 includes an internal temperature sensor. The temperature can be read in millidegrees Celsius via the in_temp0_input attribute. The in_temp0_label attribute provides the channel data path label.

/sys/bus/iio/devices/iio:device8$
cat in_temp0_label
Side-A:FDDC0->CDDC0->ADC0
/sys/bus/iio/devices/iio:device8$
cat in_temp0_input
53000

Calibration Data

What: calibration_data

The calibration_data attribute provides access to the device calibration data. This can be used to save and restore calibration across power cycles. See Calibration Data Management for detailed usage.

PFIR

The PFIR (Programmable Finite Impulse Response) configuration is defined the configuration pfilt_config (write-only).

The pfilt_config input must have the following format:

mode: <imode> <qmode>
gain: <ix> <iy> <qx> <qy>
scalar_gain: <ix> <iy> <qx> <qy>
dest: <terminal> <pfilt_sel> <bank_sel>
hc_delay: <delay>
mode_switch_en: <value>
mode_switch_add_en: <value>
real_data_mode_en: <value>
quad_mode_en: <value>
selection_mode: <mode>
<sval>
  • Each line represents a parameter or setting for the PFIR filter.

  • Lines starting with ‘#’ are considered comments and are ignored.

The format for each parameter is as follows:

  • mode: <imode> <qmode>

    Sets the mode for the PFIR filter. The <imode> and <qmode> values should be one of the predefined filter modes: disabled, real_n4, real_n2, undef, matrix, undef, complex_half, real_n.

  • gain: <ix> <iy> <qx> <qy>

    Sets the gain values for the PFIR filter. The <ix>, <iy>, <qx>, and <qy> values should be integers representing the gain in dB.

  • scalar_gain: <ix> <iy> <qx> <qy>

    Sets the scalar gain values for the PFIR filter. The <ix>, <iy>, <qx>, and <qy> values should be integers representing the scalar gain.

  • dest: <terminal> <pfilt_sel> <bank_sel>

    Sets the destination for the PFIR filter. The <terminal> value should be either rx or tx. The <pfilt_sel> value should be one of the predefined filter selects: pfilt_a0, pfilt_a1, pfilt_b0, pfilt_b1, pfilt_all, pfilt_mask. The <bank_sel> value should be one of the predefined filter banks: bank_0, bank_1, bank_2, bank_3, bank_all, bank_mask.

  • hc_delay: <delay>

    Sets the high cut delay value for the PFIR filter. The <delay> value should be an unsigned 8-bit integer.

  • mode_switch_en: <value>

    Sets the mode switch enable value for the PFIR filter. The <value> should be either 0 or 1.

  • mode_switch_add_en: <value>

    Sets the mode switch add enable value for the PFIR filter. The <value> should be either 0 or 1.

  • real_data_mode_en: <value>

    Sets the real data mode enable value for the PFIR filter. The <value> should be either 0 or 1.

  • quad_mode_en: <value>

    Sets the quad mode enable value for the PFIR filter. The <value> should be either 0 or 1.

  • selection_mode: <mode>

    Sets the profile selection mode for the PFIR filter. The <mode> value should be one of the predefined profile selection modes: direct_regmap, direct_gpio, direct_gpio1, trig_regmap, trig_gpio, trig_gpio1.

  • <sval>

    Sets the coefficient values for the PFIR filter. The <sval> value should be an integer representing the coefficient value.

CFIR

The CFIR configuration is defined by enabling [in|out]_voltage<index>_[i|q]_cfir_profile_sel, profile selection [in|out]_voltage<index>_[i|q]_cfir_profile_sel and the configuration cfir_config (write-only).

The cfir_config input must have the following format:

The cfir_config input must have the following format:

dest: <terminal> <cfir_select> <cfir_profile> <cfir_datapath>
gain: <gain_value>
complex_scalar: <scalar_i> <scalar_q>
bypass: <bypass_value>
sparse_filt_en: <sparse_filt_en_value>
32taps_en: <32taps_en_value>
coeff_transfer: <coeff_transfer_value>
enable: <enable_value> <enable_profile_value>
selection_mode: <selection_mode_value>
<cfir_coeff0_i> <cfir_coeff0_q>
<cfir_coeff1_i> <cfir_coeff1_q>
...
<cfir_coeffN_i> <cfir_coeffN_q>

Each line in the string represents a specific configuration parameter. The dest line specifies the destination terminal, CFIR select, CFIR profile, and CFIR datapath. The gain line specifies the gain value. The complex_scalar line specifies the complex scalar values. The bypass line specifies the bypass value. The sparse_filt_en line specifies the sparse filter enable value. The 32taps_en line specifies the 32 taps enable value. The coeff_transfer line specifies the coefficient transfer value. The enable line specifies the enable value and enable profile value. The selection_mode line specifies the selection mode value. The <cfir_coeff_i> and <cfir_coeff_q> lines specify the CFIR coefficient values.

/sys/bus/iio/devices/iio:device8$
ls | grep cfir
cfir_config
in_voltage0_i_cfir_en
in_voltage0_i_cfir_profile_sel
in_voltage1_i_cfir_en
in_voltage1_i_cfir_profile_sel
...
out_voltage0_i_cfir_en
out_voltage0_i_cfir_profile_sel
...
out_voltage3_q_cfir_en
out_voltage3_q_cfir_profile_sel
/sys/bus/iio/devices/iio:device8$
echo 1 > in_voltage0_i_cfir_en
/sys/bus/iio/devices/iio:device8$
cat in_voltage0_i_cfir_en
1

One main use case of CFIR is to equalize the RF carriers independent of PFILT.

Loopback

The four loopback modes are available as channel attributes. The value is always written to a side: A or B, so enabling loopback for in_voltage0 will also enable for in_voltage1.

/sys/bus/iio/devices/iio:device8$
ls | grep loopback
in_voltage0_i_loopback
in_voltage0_q_loopback
in_voltage1_i_loopback
in_voltage1_q_loopback
in_voltage2_i_loopback
in_voltage2_q_loopback
in_voltage3_i_loopback
in_voltage3_q_loopback
in_voltage_loopback_available
loopback1_blend_available
loopback1_blend_side_a
loopback1_blend_side_b
/sys/bus/iio/devices/iio:device8$
cat in_voltage_loopback_available
off loopback0 loopback1 loopback2 loopback3_jesd
/sys/bus/iio/devices/iio:device8$
echo loopback1 > in_voltage2_i_loopback
/sys/bus/iio/devices/iio:device8$
cat in_voltage3_q_loopback
loopback1

If the ADC and DAC does not have the same sampling frequency, writing will fail with -EINVAL. Consult the User Guide for all configuration requirements before enabling the loopback.

Spectrum Sniffer

The Spectrum Sniffer provides users information with fast indications of where the strong and weak signals are within the digitized signal bandwidth.

The interrupt-names fft_done_A and fft_done_B maps the spectrum sniffer interrupt for side A and B, respectively. The debug attributes for the spectrum sniffer for each side are only probed if the respective interrupt is present.

With the spectrum sniffer interrupts mapped, an additional iio device is probed and the fft properties are exposed as properties and debug properties.

~$
cd /sys/bus/iio/devices/iio:device6
/sys/bus/iio/devices/iio:device6$
ls
buffer   max_threshold  mode_available  power          uevent
buffer0  min_threshold  name            scan_elements  waiting_for_supplier
dev      mode           of_node         subsystem
  • buffer/buffer0: Allocated buffer to store and read captured data.

  • max_threshold: Maximum threshold for comparison with magnitude Output from FFT Engine.

    Default: 20
    Range: 0-255
  • min_threshold: Minimum threshold for comparison with magnitude Output from FFT Engine.

    Default: 0
    Range: 0-255
  • mode: Spectrum output mode during data capture, affects both IQ and Magnitude modes.

    normal: Normal mode - uses averaging when alpha_factor is set.
    instant: Instantaneous/Debug mode - captures single snapshot.
    Default: instant
  • mode_available: Returns all valid spectrum output modes.

  • adc_select: Select which ADC input to use for the FFT sniffer.

    adc0: ADC 0 (available on 4T4R and 8T8R)
    adc1: ADC 1 (available on 4T4R and 8T8R)
    adc2: ADC 2 (8T8R only)
    adc3: ADC 3 (8T8R only)
    Default: adc0
  • adc_select_available: Returns all valid ADC selections for the device.

Debugfs Attributes

Advanced configuration is available through debugfs. These attributes allow fine-tuning of the FFT sniffer behavior and are primarily intended for debugging and development.

~$
cd /sys/kernel/debug/iio/iio:device6
/sys/kernel/debug/iio/iio:device6$
ls
adc                   direct_reg_access  min_threshold
adc_sampling_rate_Hz  dither_enable      real_mode
alpha_factor          fft_enable_sel     run_fft_engine_background
bottom_fft_enable     fft_hold_sel       sort_enable
continuous_mode       low_power_enable   window_enable
delay_capture_ms      max_threshold

Initialization Parameters:

  • adc: ADC to configure and use for FFT capture. This is a bitmask value.

    Default: ADI_APOLLO_ADC_0
  • fft_hold_sel: Control the Sniffer fft_hold bit by SPI operation (via API function) or GPIO to hold overwriting of data to registers.

    0: Select GPIO control.
    1: Select registers control.
    Default: 0
  • fft_enable_sel: Control the Sniffer fft_enable bit by SPI operation (via API function) or GPIO to enable the FFT Engine.

    0: Select GPIO control.
    1: Select registers control.
    Default: 1
  • real_mode: Select between real and complex FFT operation.

    0: Select Complex FFT. Pair of converters used for I and Q sampling.
    1: Select Real FFT.
    Default: 0
  • max_threshold: Maximum threshold for comparison with magnitude output from FFT Engine. Same as the device property.

    Default: 255
    Range: 0-255
  • min_threshold: Minimum threshold for comparison with magnitude Output from FFT Engine.

    Default: 0
    Range: 0-255

FFT Processing Parameters:

  • sort_enable: Incoming magnitude data is sorted from least to greatest before it is stored. When sorting is disabled, magnitude data is left unsorted and is ordered by its bin number. Sorting is only available in magnitude mode.

    0: Disable.
    1: Enable.
    Default: 1
  • continuous_mode: In continuous mode, the sniffer continuously stores new data, guaranteeing that the latest data is stored. In single mode data is only stored once between the time that fft_hold is set to low, and the data is obtained. Hence, the user may miss critical data during this period in single mode. Continuous mode is only supported in magnitude mode.

    0: Single mode.
    1: Continuous mode.
    Default: 0
  • bottom_fft_enable: Each sniffer instance has one top and one bottom FFT engine that are 50% overlapped and compute in parallel. With this feature, the top and bottom FFT engine results are averaged and assist in avoiding critical time domain events

    0: Disable.
    1: Enable.
    Default: 0
  • window_enable: A hard-coded frequency domain Hamming window is applied to and is optimized for narrow spectral peaks to optimize the resolution bandwidth. in I/Q output mode, windowing will deemphasize data towards the edges of the 512-bin spectrum boundary, and thus the threshold may not be reached resulting in data not being captured.

    0: Disable.
    1: Enable.
    Default: 1
  • low_power_enable: Low power mode disables continuous mode and exponential averaging. The expected power savings for this mode is 600mW.

    0: Disable.
    1: Enable.
    Default: 1
  • dither_enable: Dither is added to input samples to reduce spurs across the spectrum.

    0: Disable.
    1: Enable.
    Default: 1

Averaging and Signal Processing:

  • alpha_factor: Exponential averaging is enabled by setting the alpha_factor between 1 and 8 and disabled when set to 0. The alpha factor sets \(\alpha\) in the equation \(y[n] = 2^{-\alpha}x[n]+(1-2^{-\alpha}y[n-1])\) and directly controls the weight of the previous sample. The average is reset to zero when data is stored or if FFT computation is stopped. Exponential averaging is only available in single mode and magnitude mode.

    0: Disable.
    1-8: Enable with specified alpha value.
    Default: 0

Capture Control:

  • run_fft_engine_background: Set to 1 for GPIO control, to skip writing the fft_enable register.

    0: Disable.
    1: Enable.
    Default: 0
  • delay_capture_ms: Delay capture by an amount of time.

    Default: 100
    Unit: ms
  • adc_sampling_rate_Hz: Read the ADC sampling rate (read-only).

The acquired data is pushed to the device’s IIO buffer.

Feature Availability by Mode

The following table shows which features are available in each sniffer mode:

FFT Sniffer Feature Matrix

Feature

Normal Mag

Instant Mag

Normal IQ

Instant IQ

sort_enable

✓

✓

✗

✗

continuous_mode

✓

✗

✗

✗

alpha_factor (averaging)

✓

✗

✗

✗

bottom_fft_enable

✓

✓

✓

✓

window_enable

✓

✓

✓

✓

dither_enable

✓

✓

✓

✓

low_power_enable

✓

✓

✓

✓

Threshold detection

✓

✓

✗

✗

FFT bins output

256

256

512

512

Modes of Operation

The spectrum sniffer supports four distinct modes of operation, determined by the combination of mode setting and channel selection (IQ vs Magnitude):

Magnitude Modes (enable in_magn0_en channel):

  1. Normal Magnitude (mode=normal): Captures magnitude spectrum with optional exponential averaging (when alpha_factor > 0), sorting (sort_enable=1), and continuous capture (continuous_mode=1). Best for ongoing spectrum monitoring.

  2. Instant Magnitude (mode=instant): Single-shot magnitude capture without averaging. Best for quick snapshots of spectrum state.

IQ Modes (enable in_voltage0_i_en and in_voltage0_q_en channels):

  1. Normal IQ (mode=normal): Captures complex I/Q FFT data. Sorting, continuous mode, and exponential averaging are not available in IQ mode. Best for detailed spectral analysis requiring phase information.

  2. Instant IQ (mode=instant): Single-shot complex I/Q capture. Best for debug and calibration purposes.

Note

The mode is automatically determined based on which channels are enabled in scan_elements/. Enabling the magnitude channel selects magnitude mode, while enabling I/Q channels selects IQ mode.

IIO Channels

The FFT sniffer exposes the following IIO channels:

  • in_index: FFT bin index (0-255 for real mode, 0-511 for complex mode)

  • in_voltage0_i: In-phase (I) FFT data for IQ mode

  • in_voltage0_q: Quadrature (Q) FFT data for IQ mode

  • in_magn0: Magnitude FFT data for magnitude mode

Channel Scan Masks - valid combinations:

  • Index + I + Q: For IQ mode captures (in_index_en=1, in_voltage0_i_en=1, in_voltage0_q_en=1)

  • Index + Magnitude: For magnitude mode captures (in_index_en=1, in_magn0_en=1)

Data Format

Magnitude Mode (real FFT, 256 bins):

Each sample contains:

  • Bin index (9 bits unsigned, 0-255)

  • Magnitude value (9 bits unsigned)

IQ Mode (complex FFT, 512 bins):

Each sample contains:

  • Bin index (9 bits unsigned, 0-511)

  • I data (9 bits signed)

  • Q data (9 bits signed)

All values are packed into 16-bit little-endian format.

Example Usage

Capture Magnitude Spectrum:

# Configure for magnitude mode with sorting
~$
cd /sys/bus/iio/devices/iio:device6
/sys/bus/iio/devices/iio:device6$
echo normal > mode
/sys/bus/iio/devices/iio:device6$
echo 1 > /sys/kernel/debug/iio/iio:device6/sort_enable

# Enable magnitude channels
/sys/bus/iio/devices/iio:device6$
echo 1 > scan_elements/in_index_en
/sys/bus/iio/devices/iio:device6$
echo 1 > scan_elements/in_magn0_en

# Configure and enable buffer
/sys/bus/iio/devices/iio:device6$
echo 256 > buffer0/length
/sys/bus/iio/devices/iio:device6$
echo 1 > buffer0/enable

# Capture data
/sys/bus/iio/devices/iio:device6$
cat /dev/iio:device6 | head -c 1024 > spectrum.bin

Capture IQ Spectrum:

# Configure for IQ mode
~$
cd /sys/bus/iio/devices/iio:device6
/sys/bus/iio/devices/iio:device6$
echo instant > mode

# Enable IQ channels
/sys/bus/iio/devices/iio:device6$
echo 1 > scan_elements/in_index_en
/sys/bus/iio/devices/iio:device6$
echo 1 > scan_elements/in_voltage0_i_en
/sys/bus/iio/devices/iio:device6$
echo 1 > scan_elements/in_voltage0_q_en

# Configure and enable buffer
/sys/bus/iio/devices/iio:device6$
echo 512 > buffer0/length
/sys/bus/iio/devices/iio:device6$
echo 1 > buffer0/enable

# Capture data
/sys/bus/iio/devices/iio:device6$
cat /dev/iio:device6 | head -c 3072 > iq_spectrum.bin

Fast Frequency Hopping

The NCO frequency and phase settings can be stored as a set of up-to 32 profiles, each with a 32-bit FTW and 16-bit phase offset word, to be selectively assigned to the NCO during runtime. This allows to quickly change (hop) the NCO frequency, known as Fast Frequency Hopping (FFH).

Tx FFH FNCO

The user configures the NCO FFH frequency by writing the index (0 to 31) to out_voltageX_[i|q]_ffh_fnco_index followed by the frequency value to out_voltageX_[i|q]_ffh_fnco_frequency, for example:

/sys/bus/iio/devices/iio:device8$
echo 1 > out_voltage0_i_ffh_fnco_index
/sys/bus/iio/devices/iio:device8$
echo $((16#20000000)) > out_voltage0_ffh_fnco_frequency

Then hop to the desired frequency writing the index to out_voltageX_[i|q]_ffh_fnco_select, and write -1 to disable the feature; for example:

Important

If the trigger mode is not set to 4 (ADI_APOLLO_NCO_CHAN_SEL_DIRECT_REGMAP), the method will return -EINVAL;

/sys/bus/iio/devices/iio:device8$
echo 1 > out_voltage0_i_ffh_fnco_select
Tx FFH CNCO

The user configures the NCO FFH frequency by writing the index (0 to 15) to out_voltageX_[i|q]_ffh_cnco_index followed by the frequency value to out_voltageX_[i|q]_ffh_cnco_frequency, for example:

/sys/bus/iio/devices/iio:device8$
echo 1 > out_voltage0_i_ffh_cnco_index
/sys/bus/iio/devices/iio:device8$
echo $((16#20000000)) > out_voltage0_ffh_cnco_frequency

Then hop to the desired frequency writing the index to out_voltageX_[i|q]_ffh_cnco_select, for example:

/sys/bus/iio/devices/iio:device8$
echo 1 > out_voltage0_i_ffh_fnco_select

out_voltageX_[i|q]_ffh_cnco_frequency at index 0 is equivalent to in_voltage0_i_main_nco_frequency

Trigger mode

By default, the profile will hop on the register access for the profile set call. Other options are available and configurable with out_voltageX_[i|q]_ffh_fnco_mode.

The options are:

  • 0: ADI_APOLLO_NCO_CHAN_SEL_TRIG_AUTO, Trigger based hopping, auto Hopping Mode.

  • 1: ADI_APOLLO_NCO_CHAN_SEL_TRIG_REGMAP, Trigger based hopping, scheduled Regmap.

  • 2: ADI_APOLLO_NCO_CHAN_SEL_TRIG_GPIO, Trigger based hopping, scheduled GPIO.

  • 3: ADI_APOLLO_NCO_CHAN_SEL_DIRECT_GPIO, Direct GPIO profile select, all params hop together.

  • 4: ADI_APOLLO_NCO_CHAN_SEL_DIRECT_REGMAP, Direct spi/hsci nco profile select, all params hop together (default).

For example:

/sys/bus/iio/devices/iio:device8$
echo 1 > out_voltage0_i_ffh_fnco_mode
Rx FFH FNCO

The RX path also supports Fast Frequency Hopping. The user configures the NCO FFH frequency by writing the index (0 to 31) to in_voltageX_[i|q]_ffh_fnco_index followed by the frequency value to in_voltageX_[i|q]_ffh_fnco_frequency, for example:

/sys/bus/iio/devices/iio:device8$
echo 1 > in_voltage0_i_ffh_fnco_index
/sys/bus/iio/devices/iio:device8$
echo 500000000 > in_voltage0_i_ffh_fnco_frequency

Then hop to the desired frequency writing the index to in_voltageX_[i|q]_ffh_fnco_select, and write -1 to disable the feature:

/sys/bus/iio/devices/iio:device8$
echo 1 > in_voltage0_i_ffh_fnco_select

The trigger mode is configured via in_voltageX_[i|q]_ffh_fnco_mode.

Rx FFH CNCO

The user configures the coarse NCO FFH frequency by writing the index (0 to 31) to in_voltageX_[i|q]_ffh_cnco_index followed by the frequency value to in_voltageX_[i|q]_ffh_cnco_frequency:

/sys/bus/iio/devices/iio:device8$
echo 1 > in_voltage0_i_ffh_cnco_index
/sys/bus/iio/devices/iio:device8$
echo 1000000000 > in_voltage0_i_ffh_cnco_frequency

Then hop to the desired frequency writing the index to in_voltageX_[i|q]_ffh_cnco_select:

/sys/bus/iio/devices/iio:device8$
echo 1 > in_voltage0_i_ffh_cnco_select

The trigger mode is configured via in_voltageX_[i|q]_ffh_cnco_mode.

Buffer Memory (BMEM) Interface

The AD9088 contains on-chip buffer memory (BMEM) that can be used for data capture and playback. The driver exposes a separate IIO device for BMEM operations, named ad9088-bmem (or with a device-specific label suffix).

Overview:

  • 128KB SRAM per BMEM instance (32K 32-bit words)

  • 8 BMEM instances in 8T8R mode (A0-A3, B0-B3), 4 in 4T4R mode (A0-A1, B0-B1)

  • Supports sample delay configuration for data path alignment

  • Supports frequency hopping delay profiles

IIO Device Registration:

The BMEM interface registers as a separate IIO device with channels corresponding to each ADC path:

  • 8T8R mode: 8 channels (0-3 for Side A, 4-7 for Side B)

  • 4T4R mode: 4 channels (0-1 for Side A, 2-3 for Side B)

~$
ls /sys/bus/iio/devices/
iio:device8    # Main AD9088 device
iio:device9    # BMEM device (ad9088-bmem or <label>-bmem)

Channel Attributes:

Each BMEM channel exposes the following sysfs attributes:

~$
ls /sys/bus/iio/devices/iio:device9/
buffer/
in_voltage0_delay_hop_array
in_voltage0_delay_hop_parity_check_en
in_voltage0_delay_hop_sel_mode
in_voltage0_delay_hop_trig_sclr_en
in_voltage0_delay_sample
in_voltage0_delay_sample_config_value
in_voltage0_delay_sample_parity_check_en
in_voltage0_delay_start
in_voltage0_sampling_frequency
...
scan_elements/
BMEM Channel Attributes

Sample Delay Configuration:

  • in_voltageX_delay_sample: Set the sample delay value directly. This is a simplified interface for setting the delay without other configuration options.

    Range: 0-65535 (16-bit)
    Default: 0
    # Set 100 sample delay on channel 0
    
    $
    
    echo 100 > in_voltage0_delay_sample
    
    $
    
    cat in_voltage0_delay_sample
    
    100
    
  • in_voltageX_delay_sample_config_value: Set the sample delay value through the full configuration structure. Updates the delay and applies parity settings.

    Range: 0-65535 (16-bit)
    Default: 0
  • in_voltageX_delay_sample_parity_check_en: Enable or disable parity checking for sample delay mode.

    0: Disable parity check
    1: Enable parity check (default)

Frequency Hopping Delay Configuration:

For fast frequency hopping applications, BMEM supports 4 delay profiles that can be cycled through or selected via GPIO.

  • in_voltageX_delay_hop_array: Configure all 4 delay hop profiles at once. Write 4 space-separated values (one per profile).

    Format: <delay0> <delay1> <delay2> <delay3>
    Range per value: 0-65535 (16-bit)
    Default: 0 0 0 0
    # Set hop delay profiles: 0, 100, 200, 300
    
    $
    
    echo "0 100 200 300" > in_voltage0_delay_hop_array
    
    $
    
    cat in_voltage0_delay_hop_array
    
    0 100 200 300
    
  • in_voltageX_delay_hop_sel_mode: Select how hop profiles are chosen.

    0: Cycle through profiles sequentially (0→1→2→3→0…)
    1: GPIO selects next profile
    Default: 0
  • in_voltageX_delay_hop_trig_sclr_en: Enable trigger mode self-clear. When enabled, the trigger automatically clears after activation.

    0: Disable self-clear
    1: Enable self-clear (default)
  • in_voltageX_delay_hop_parity_check_en: Enable or disable parity checking for hop delay mode.

    0: Disable parity check
    1: Enable parity check (default)
  • in_voltageX_delay_start: Trigger the delay operation for this channel’s BMEM. Write 1 to start the delay operation. Read always returns 0.

    # Trigger delay start on channel 0
    
    $
    
    echo 1 > in_voltage0_delay_start
    

Sampling Frequency:

  • in_voltageX_sampling_frequency: Read the ADC sampling rate for this channel (read-only). Value is in Hz.

    $
    
    cat in_voltage0_sampling_frequency
    
    2949120000
    
BMEM Buffer Operations

The BMEM device supports IIO buffer operations for capturing ADC samples.

Enabling Capture:

# Enable channels for capture
$
echo 1 > /sys/bus/iio/devices/iio:device9/scan_elements/in_voltage0_en
$
echo 1 > /sys/bus/iio/devices/iio:device9/scan_elements/in_voltage1_en

# Set buffer length (samples per channel)
$
echo 8192 > /sys/bus/iio/devices/iio:device9/buffer/length

# Enable buffer to start capture
$
echo 1 > /sys/bus/iio/devices/iio:device9/buffer/enable

# Read captured data
$
cat /dev/iio:device9 > captured_data.bin

# Disable buffer
$
echo 0 > /sys/bus/iio/devices/iio:device9/buffer/enable

Data Format:

Captured samples are 16-bit signed values in little-endian format. When multiple channels are enabled, samples are interleaved in channel order.

GPIOs & GPIO chip

The device contains 30 general purpose GPIOs that can be used to trigger various changes and can be exported into a gpio_chip using the adi,gpio-exports devicetree property:

trx0_ad9084: ad9084@0 {
     adi,gpio-exports = /bits/ 8 <15 16 17 18>;
};

Some of the device GPIOs are mapped in the HDL design to a axi_gpio IP Core, and the apollo’s and axi_gpio’s can be attached to other drivers in the device tree:

Tip

0 is the index of item in the adi,gpio-exports, and in the previous example, is equivalent to the device’s GPIO 15. Also ensure to check the schematics and HDL design for the routes between apollo’s GPIO, axi_gpio’s and other input options.

my_driver {
     /* ... */
     provider-gpios = <&axi_gpio 0 GPIO_ACTIVE_HIGH>;
     consumer-gpios = <&tx0_ad9084 0 GPIO_ACTIVE_HIGH>;
}

Or from user space through gpiod:

~$
gpiodetect
gpiochip0 [a4000000.gpio] (64 lines)
gpiochip1 [versal_gpio] (58 lines)
gpiochip2 [pmc_gpio] (116 lines)
gpiochip3 [ad9088] (4 lines)
~$
gpioget ad9088 3
0
~$
gpioset a4000000.gpio 3=1
~$
gpioget ad9088 3
1

Debug system

An additional debug interface is provided through debugfs:

~$
cd /sys/kernel/debug/iio/iio\:device8 ; pwd
/sys/kernel/debug/iio/iio:device8
/sys/kernel/debug/iio/iio:device8$
ls
api_version                 jrx_phase_adjust_calc       mcs_fg_track_cal_run
bist_2d_eyescan_jrx         jtx_lane_drive_swing        mcs_init
bist_prbs_error_counters_jrx jtx_lane_post_emphasis     mcs_init_cal_status
bist_prbs_select_jrx        jtx_lane_pre_emphasis       mcs_track_cal_setup
bist_prbs_select_jtx        mcs_bg_track_cal_freeze     mcs_track_status
chip_version                mcs_bg_track_cal_run        misc
clk_pwr_stat                mcs_cal_run                 pseudorandom_err_check
die_id                      mcs_dt0_measurement         status
direct_reg_access           mcs_dt1_measurement         temperature_status
hsci_enable                 mcs_dt_restore              uuid

Communication Protocol

  • hsci_enable: Select communication protocol for register access.

    0: SPI protocol
    1: HSCI protocol (High-Speed Communication Interface)
$
cat hsci_enable
1
$
echo 0 > hsci_enable
$
cat hsci_enable
0

MCS Calibration

Multi-Chip Synchronization (MCS) calibration is used for synchronizing multiple AD9088 devices to achieve ±10ps alignment accuracy. The MCS flow uses BSYNC Time-of-Flight (ToF) measurements to compensate for path delays between the ADF4030 precision synchronizer and each Apollo device.

MCS calibration is performed automatically by the driver during initialization when the io-channels property with bsync and clk channel references are defined in the Apollo device tree node:

trx0_ad9084: ad9088@0 {
    compatible = "adi,ad9088";
    /* ... other properties ... */
    io-channels = <&adf4030 5>, <&adf4382 0>;
    io-channel-names = "bsync", "clk";

    /* Optional: TDC decimation rate (default: 1023) */
    adi,mcs-track-decimation = /bits/ 16 <1023>;
};

Automatic MCS Flow (per UG-2300):

When io-channels are configured, the driver automatically performs:

  1. BSYNC Time-of-Flight Measurement: Measures round-trip path delay between ADF4030 and Apollo using delta-T0 and delta-T1 measurements.

  2. Path Delay Compensation: Calculates and applies negative phase offset to the ADF4030 output channel to compensate for cable and PCB trace delays.

  3. MCS Init Calibration: Aligns internal SYSREF to external SYSREF within ±0.4 clock cycles. The driver validates the calibration and returns an error if alignment fails.

  4. Tracking Calibration Setup: Configures the TDC decimation rate (from device tree or default 1023) and enables tracking.

  5. ADF4382 Auto-Align: Enables the ADF4382’s automatic phase alignment feature for continuous synchronization.

  6. Foreground Tracking Calibration: Runs initial tracking calibration to establish baseline phase correction values.

  7. Background Tracking Calibration: Starts continuous background tracking to maintain synchronization over time and temperature.

Note

Dual Clock Mode Limitation: MCS tracking calibration is only supported in single clock mode due to hardware limitations. In dual clock mode, the driver performs MCS init calibration for both A-side and B-side, but skips tracking calibration.

Driver Validation and Warnings:

The driver performs several validation checks during MCS calibration:

  • MCS Init Cal Failure: If init calibration fails (SYSREF not locked or alignment outside tolerance), the driver returns an error and stops the JESD204 state machine.

  • Trigger Phase Margin: Warns if trigger phase is outside 25%-75% of the SYSREF period, which may cause ±1 cycle latency jitter.

  • Path Delay Sanity Check: Warns if calculated path delay is very small (<5% of period) or near maximum (>45% of period), indicating potential hardware issues.

For manual control or debugging, MCS calibration attributes are also available through debugfs.

Available debugfs attributes:

$
ls /sys/kernel/debug/iio/iio:device8/mcs_*
mcs_bg_track_cal_freeze  mcs_dt1_measurement    mcs_init
mcs_bg_track_cal_run     mcs_dt_restore         mcs_init_cal_status
mcs_cal_run              mcs_fg_track_cal_run   mcs_track_cal_setup
mcs_dt0_measurement      mcs_track_cal_validate mcs_track_status

Delta-T Measurement:

  • mcs_dt0_measurement: Trigger delta-T0 measurement. Write 1 to run. Read returns the measured delta-T value in picoseconds.

  • mcs_dt1_measurement: Trigger delta-T1 measurement. Write 1 to run. Read returns the measured delta-T value in picoseconds.

  • mcs_dt_restore: Restore delta-T measurement. Write 1 to restore.

Initial Calibration:

  • mcs_init: Initialize MCS calibration. Write 1 to setup.

  • mcs_cal_run: Run MCS initial calibration. Write 1 to execute. Read returns Passed or Failed based on calibration status.

  • mcs_init_cal_status: Read-only. Returns detailed initial calibration status including per-side ADC and phase correction results.

Tracking Calibration:

  • mcs_track_cal_setup: Setup tracking calibration. Write 1 to configure.

  • mcs_fg_track_cal_run: Run foreground tracking calibration. Write 1 to execute. Foreground calibration runs once and blocks until complete.

  • mcs_bg_track_cal_run: Control background tracking calibration. Write 1 to start, 0 to abort. Read returns current run state.

  • mcs_bg_track_cal_freeze: Freeze/unfreeze background tracking calibration. Write 1 to freeze, 0 to unfreeze. Read returns current freeze state. Only valid when background tracking is running.

  • mcs_track_status: Read-only. Returns tracking calibration status including iteration count, phase errors, and per-ADC correction values.

  • mcs_track_cal_validate: Read-only. Validates that MCS tracking calibration values in Apollo firmware match the ADF4382 hardware bleed current values. Use this to verify that tracking calibration is maintaining synchronization.

    $
    
    cat mcs_track_cal_validate
    
    MCS Tracking Cal Validation:
      ADF4382 HW:  bleed_pol=0 coarse=5 fine=128
      Apollo FW:   bleed_pol=0 coarse=5 fine=128
      Status:      SYNCHRONIZED
    

    If values don’t match, check for hardware issues or tracking calibration faults.

Manual MCS Calibration Sequence:

When MCS is not automatically configured via device tree io-channels, the full MCS calibration sequence requires coordination between the Apollo device, the ADF4030 SYSREF generator, and the ADF4382 clock source. The sequence involves delta-T measurements to calculate path delay and phase compensation.

Warning

The BSYNC signal direction must be carefully managed to avoid bus contention. Both Apollo and ADF4030 can drive this signal. The apollo_sysref_X_output_enable attribute controls the direction: when enabled (1), ADF4030 drives BSYNC to Apollo; when disabled (0), Apollo drives BSYNC back to ADF4030 for the return path measurement. Failure to sequence this correctly may result in signal contention and incorrect measurements.

The following example shows the complete MCS sequence for a single Apollo device (device index 0). In a multi-device system, repeat this sequence for each device.

# Set paths for Apollo, ADF4030, and ADF4382
APOLLO=/sys/kernel/debug/iio/iio:deviceX
ADF4030=/sys/bus/iio/devices/iio:deviceY
ADF4382=/sys/bus/iio/devices/iio:deviceZ

# Step 1: Enable SYSREF output and initialize MCS
echo 1 > $ADF4030/apollo_sysref_0_output_enable
echo 1 > $APOLLO/mcs_init

# Step 2: Delta-T0 measurement (with SYSREF enabled)
echo 1 > $APOLLO/mcs_dt0_measurement
apollo_delta_t0=$(cat $APOLLO/mcs_dt0_measurement)
adf4030_delta_t0=$(cat $ADF4030/apollo_sysref_0_phase)

# Step 3: Disable SYSREF output for Delta-T1 measurement
echo 0 > $ADF4030/apollo_sysref_0_output_enable

# Step 4: Delta-T1 measurement (Apollo driving BSYNC back to ADF4030)
echo 1 > $APOLLO/mcs_dt1_measurement
apollo_delta_t1=$(cat $APOLLO/mcs_dt1_measurement)
adf4030_delta_t1=$(cat $ADF4030/apollo_sysref_0_phase)

# Step 5: Restore delta-T state
echo 1 > $APOLLO/mcs_dt_restore

# Step 6: Calculate path delay (values in femtoseconds)
# bsync_period = 1e15 / sysref_frequency
# calc_delay = (adf4030_delta_t0 - adf4030_delta_t1) - (apollo_delta_t1 - apollo_delta_t0)
# round_trip_delay = (calc_delay + bsync_period) % bsync_period
# path_delay = round_trip_delay / 2

# Step 7: Re-enable SYSREF and apply phase compensation
echo 1 > $ADF4030/apollo_sysref_0_output_enable
echo -$path_delay > $ADF4030/apollo_sysref_0_phase

# Step 8: Run MCS initial calibration
echo 1 > $APOLLO/mcs_cal_run
cat $APOLLO/mcs_cal_run  # Should show "Passed"

# Step 9: Setup tracking calibration (single clock mode only)
echo 1 > $APOLLO/mcs_track_cal_setup

# Step 10: Enable ADF4382 auto-align for automatic phase adjustment
# Note: No explicit phase value is set - auto-align handles this automatically
echo 1 > $ADF4382/out_altvoltage0_en_auto_align

# Step 11: Run foreground tracking calibration, then start background tracking
echo 1 > $APOLLO/mcs_fg_track_cal_run
echo 1 > $APOLLO/mcs_bg_track_cal_run

# Step 12: Verify calibration status
cat $APOLLO/mcs_init_cal_status
cat $APOLLO/mcs_track_status

# Step 13: (Optional) Validate tracking cal synchronicity
cat $APOLLO/mcs_track_cal_validate

Checking Calibration Status:

$
cat mcs_init_cal_status
$
cat mcs_track_status

Stopping Background Tracking Calibration:

$
echo 0 > mcs_bg_track_cal_run

Device Information

Attributes for reading device identification and version information.

  • api_version: Read the Apollo API version.

    $
    
    cat api_version
    
    1.10.0
    
  • chip_version: Read chip version, revision, and grade.

    $
    
    cat chip_version
    
    AD9084 Rev. 4 Grade 3
    
  • die_id: Read the die identification number.

    $
    
    cat die_id
    
    DieID 9
    
  • uuid: Read the unique device identifier (128-bit).

    $
    
    cat uuid
    
    334d0b28248a328c8e4abc27eb592153
    

Temperature Monitoring

  • temperature_status: Read detailed temperature measurements from all on-chip thermal sensors.

    $
    
    cat temperature_status
    
    TMU (deg C): serdes_pll=47 mpu_a=52 mpu_b=53 adc_a=58 clk_a=51 adc_b=61 clk_b=53 clk_c=51 (avg: 53, avg mask: 0x01fe)
    

    The output shows temperatures in degrees Celsius for:

    • serdes_pll: SERDES PLL temperature

    • mpu_a/mpu_b: Microprocessor unit A/B temperatures

    • adc_a/adc_b: ADC A/B temperatures

    • clk_a/clk_b/clk_c: Clock domain temperatures

    • avg: Averaged temperature

    • avg mask: Bitmask indicating which sensors are included in the average

Clock Power Status

  • clk_pwr_stat: Read clock input power detection status.

    $
    
    cat clk_pwr_stat
    
    Clock input power detection A: GOOD
    Clock input power detection B: UNUSED
    

    Status values: GOOD, UNUSED, or power-related status indicators.

JESD204 BIST (Built-In Self-Test)

The BIST subsystem provides PRBS (Pseudo-Random Binary Sequence) testing for JESD204 link integrity verification.

PRBS Pattern Selection:

  • bist_prbs_select_jrx: Select PRBS pattern for JRX (receive) testing. Write the PRBS polynomial order to enable, or 0 to disable.

    0: Disable PRBS checker
    7: PRBS7 pattern
    9: PRBS9 pattern
    15: PRBS15 pattern
    31: PRBS31 pattern
    # Enable PRBS7 checker
    
    $
    
    echo 7 > bist_prbs_select_jrx
    
    # Disable PRBS checker
    
    $
    
    echo 0 > bist_prbs_select_jrx
    
  • bist_prbs_select_jtx: Select PRBS pattern for JTX (transmit) testing. Write the PRBS polynomial order to enable, or 0 to disable.

    0: Disable PRBS generator
    7: PRBS7 pattern
    9: PRBS9 pattern
    15: PRBS15 pattern
    31: PRBS31 pattern
    # Enable PRBS31 generator
    
    $
    
    echo 31 > bist_prbs_select_jtx
    

PRBS Error Counters:

  • bist_prbs_error_counters_jrx: Read PRBS error counters for all JRX lanes. Shows errors/total for each active lane. Read-only.

    $
    
    cat bist_prbs_error_counters_jrx
    
    A: lane-5 0/0
    A: lane-1 0/0
    A: lane-3 0/0
    A: lane-7 0/0
    B: lane-1 0/0
    B: lane-7 0/0
    B: lane-10 0/0
    B: lane-3 0/0
    

JESD Eye Scan:

  • bist_2d_eyescan_jrx: Trigger a 2D eye scan for JRX SERDES lanes. Write lane parameters to initiate the scan; read returns eye diagram data.

    Write format: <lane> [prbs] [duration_ms]

    lane: Physical lane number (0-23, where 0-11 is side A, 12-23 is side B)
    prbs: PRBS pattern (7, 9, 15, or 31). Default: 7
    duration_ms: Measurement duration in milliseconds. Default: 10
    # Scan lane 1 with PRBS7
    
    $
    
    echo 1 > bist_2d_eyescan_jrx
    
    # Scan lane 5 with PRBS31 and 100ms duration
    
    $
    
    echo "5 31 100" > bist_2d_eyescan_jrx
    
    $
    
    cat bist_2d_eyescan_jrx
    
    # lane 5 spo_steps 16 rate 24750000 spo_left 12 spo_right 12 version 1
    -16,100,-100
    -15,104,-104
    ...
    

JTX Lane Configuration

Configure JESD204 transmit lane signal integrity parameters. Each attribute takes three space-separated values: <link_side_mask> <lane> <value>.

Link side mask values:

1: Side A only (ADI_APOLLO_LINK_SIDE_A)
4: Side B only (ADI_APOLLO_LINK_SIDE_B)
5: Both sides (ADI_APOLLO_LINK_SIDE_ALL)

Lane number: Physical lane index 0-11 (per side).

  • jtx_lane_drive_swing: Set the output drive swing level for JTX lanes.

    0: 1000 mV swing (ADI_APOLLO_SER_SWING_1000)
    1: 850 mV swing (ADI_APOLLO_SER_SWING_850)
    2: 750 mV swing (ADI_APOLLO_SER_SWING_750)
    3: 500 mV swing (ADI_APOLLO_SER_SWING_500)
    # Set lane 3 on both sides to 850mV swing
    
    $
    
    echo "5 3 1" > jtx_lane_drive_swing
    
  • jtx_lane_pre_emphasis: Set pre-emphasis for JTX lanes to compensate for high-frequency signal loss.

    0: 0 dB pre-emphasis (ADI_APOLLO_SER_PRE_EMP_0DB)
    1: 3 dB pre-emphasis (ADI_APOLLO_SER_PRE_EMP_3DB)
    2: 6 dB pre-emphasis (ADI_APOLLO_SER_PRE_EMP_6DB)
    # Set lane 5 on side A to 3dB pre-emphasis
    
    $
    
    echo "1 5 1" > jtx_lane_pre_emphasis
    
  • jtx_lane_post_emphasis: Set post-emphasis (de-emphasis) for JTX lanes.

    0: 0 dB post-emphasis (ADI_APOLLO_SER_POST_EMP_0DB)
    1: 3 dB post-emphasis (ADI_APOLLO_SER_POST_EMP_3DB)
    2: 6 dB post-emphasis (ADI_APOLLO_SER_POST_EMP_6DB)
    3: 9 dB post-emphasis (ADI_APOLLO_SER_POST_EMP_9DB)
    4: 12 dB post-emphasis (ADI_APOLLO_SER_POST_EMP_12DB)
    # Set lane 7 on side B to 6dB post-emphasis
    
    $
    
    echo "4 7 2" > jtx_lane_post_emphasis
    

JRX Phase Adjustment

  • jrx_phase_adjust_calc: Trigger JRX phase adjustment calculation for JESD204 link synchronization. Write any value to trigger calculation; read returns the calculated phase adjustment value.

Pseudorandom Error Check

  • pseudorandom_err_check: Read the pseudorandom number (PN) sequence checker status for all digital channels. Used to verify data path integrity.

    $
    
    cat pseudorandom_err_check
    
    CH0 : PN9 : Out of Sync : PN Error
    CH1 : PN9 : Out of Sync : PN Error
    CH2 : PN9 : Out of Sync : PN Error
    CH3 : PN9 : Out of Sync : PN Error
    CH4 : PN9 : Out of Sync : PN Error
    CH5 : PN9 : Out of Sync : PN Error
    CH6 : PN9 : Out of Sync : PN Error
    CH7 : PN9 : Out of Sync : PN Error
    CH8 : UNDEF : In Sync : PN Error
    CH9 : UNDEF : In Sync : PN Error
    CH10 : UNDEF : In Sync : PN Error
    CH11 : UNDEF : In Sync : PN Error
    CH12 : UNDEF : In Sync : PN Error
    CH13 : UNDEF : In Sync : PN Error
    CH14 : UNDEF : In Sync : PN Error
    CH15 : UNDEF : In Sync : PN Error
    CH16 : UNDEF : In Sync : PN Error
    

    Each line shows:

    • Channel number (CHx)

    • PN sequence type (PN9, PN23, UNDEF, etc.)

    • Sync status (In Sync / Out of Sync)

    • Error status (PN Error / OK)

Miscellaneous

  • misc: General-purpose miscellaneous register for debug operations.

  • direct_reg_access: Standard IIO debugfs attribute for direct SPI register read/write access. Useful for low-level debugging.

    # Read register 0xF0
    
    $
    
    echo 0xF0 > direct_reg_access
    
    $
    
    cat direct_reg_access
    
    0xF0
    

Calibration Data Management

The AD9088 driver provides a comprehensive calibration data management system that allows you to save and restore device calibration across power cycles. This significantly reduces boot time and maintains consistent performance.

Overview

During normal device initialization, the AD9088 performs extensive calibration of ADCs, SERDES transceivers, and clock conditioning. This process can take considerable time. The calibration data management feature allows you to:

  • Save all calibration data to a binary file

  • Restore calibration data from file during driver probe

  • Skip time-consuming calibration procedures on subsequent boots

  • Maintain factory or field calibration data

Calibration Data Components

The calibration system saves the following data:

  • ADC Calibration: Sequential and random mode calibration for all ADCs

  • SERDES RX Calibration: Calibration for all SERDES RX 12-packs

  • Clock Conditioning Calibration: Clock conditioning calibration for both sides

File Format

Calibration data is stored in a structured binary format with:

  • Magic Number: 0x41443930 (“AD90”) for file identification

  • Version: Format version (currently 2)

  • Device Metadata: Chip ID (AD9084/AD9088) and configuration (4T4R/8T8R)

  • Section Headers: Offsets and sizes for each calibration component

  • CRC32 Checksum: Data integrity validation

Sysfs Interface

Calibration data is accessed via a binary sysfs attribute:

/sys/bus/iio/devices/iio:deviceX/calibration_data

Saving Calibration Data

After device initialization and calibration, save the calibration data:

$
cat /sys/bus/iio/devices/iio:device8/calibration_data > /lib/firmware/ad9088_cal.bin
$
ls -lh /lib/firmware/ad9088_cal.bin
-rw-r--r-- 1 root root 100K Feb 11 15:30 /lib/firmware/ad9088_cal.bin

The save operation:

  1. Freezes ADC and SERDES background calibration

  2. Updates firmware CRC

  3. Reads all calibration data (ADC, SERDES RX, Clock Conditioning)

  4. Builds binary file with header and CRC32

  5. Unfreezes background calibration

Restoring Calibration Data

To manually restore calibration data:

$
cat /lib/firmware/ad9088_cal.bin > /sys/bus/iio/devices/iio:device8/calibration_data

The restore operation validates:

  • Magic number and file format version

  • Chip ID matches current device

  • Device configuration (4T4R/8T8R) matches

  • CRC32 integrity

Note

Large calibration files are automatically handled via multi-write accumulation (kernel typically splits large writes into 4KB chunks).

Automatic Calibration Load

For automatic calibration restore during driver probe, add the calibration firmware property to your device tree:

&spi0 {
    trx0_ad9084: ad9088@ {
        compatible = "adi,ad9088";
        reg = <0>;
        spi-max-frequency = <10000000>;

        /* Automatically load calibration data at boot */
        adi,device-calibration-data-name = "ad9088_cal.bin";

        /* ... other properties ... */
    };
};

When this property is present, the driver will:

  1. Request the firmware file from /lib/firmware/ during probe

  2. Validate the calibration data

  3. Restore calibration to hardware

  4. Continue with normal device initialization

If the property is not present, the driver performs normal initialization with full calibration.

Important

  • The calibration file must be placed in /lib/firmware/ before boot

  • If the file is missing or invalid, driver probe will fail

  • Calibration data is loaded after firmware but before other HW configuration

  • Calibration data must match the device (same chip ID and configuration)

Calibration Dump Tool

A standalone utility ad9088_cal_dump is provided for inspecting calibration files:

$cd drivers/iio/adc/apollo/tools
$make
$./ad9088_cal_dump /lib/firmware/ad9088_cal.bin

The tool displays:

  • File size and CRC validation status

  • Header information (magic, version, chip ID, configuration)

  • Section offsets and sizes

  • Data preview (first 16 bytes of each section)

  • Warnings for uninitialized or corrupted data

Example output:

File: /lib/firmware/ad9088_cal.bin
Size: 102464 bytes

=== CRC Validation ===

Stored CRC:     0x12345678
Calculated CRC: 0x12345678
Status:         [OK]

=== AD9088 Calibration Data Header ===

Magic Number:        0x41443930 ('AD90') [OK]
Version:             1 [OK]
Chip ID:             0x9088 (AD9088)
Configuration:       8T8R (8 TX, 8 RX)
Number of ADCs:      8
Number of DACs:      8
Number of SERDES RX: 4
Number of SERDES TX: 4

=== Calibration Sections ===

ADC Calibration:
  Offset: 0x00000040 (64 bytes)
  Size:   0x0000C800 (51200 bytes)
  Per Mode: 25600 bytes
  Per ADC:  3200 bytes

[... additional sections ...]

Error Handling

Common Errors

Error

Cause

Solution

Invalid magic

Wrong file format

Use file saved by this driver

Version mismatch

Incompatible format version

Re-save calibration with current driver

Chip ID mismatch

File from different device

Use calibration from same chip type

Config mismatch

4T4R vs 8T8R mismatch

Use calibration from same device config

CRC error

File corruption

Re-save calibration data

Size mismatch

Truncated file

Check file was completely written

Debugging

Enable kernel debug messages:

$
echo 8 > /proc/sys/kernel/printk
$
echo 'file ad9088_cal.c +p' > /sys/kernel/debug/dynamic_debug/control
$
dmesg | grep -i "calibration\|ad9088"

Successful save output:

ad9088 spi1.0: Saving calibration data...
ad9088 spi1.0: SERDES JRX enabled mask: 0x0003
ad9088 spi1.0: Freezing ADC background calibration...
ad9088 spi1.0: Freezing SERDES JRX background calibration (mask: 0x0003)...
ad9088 spi1.0: Updating calibration data CRC...
ad9088 spi1.0: CRC update status: 0
ad9088 spi1.0: Reading ADC calibration data...
ad9088 spi1.0: Unfreezing ADC background calibration...
ad9088 spi1.0: Unfreezing SERDES JRX background calibration...
ad9088 spi1.0: Reading SERDES RX calibration data...
ad9088 spi1.0: Reading clock conditioning calibration data...
ad9088 spi1.0: Calibration data saved: 60708 bytes (ADC: 58624, SERDES RX: 1760, Clk Cond: 240)

Successful restore output:

ad9088 spi1.0: Starting calibration restore: 60708 bytes expected
ad9088 spi1.0: All calibration data received, restoring...
ad9088 spi1.0: Restoring calibration data...
ad9088 spi1.0: SERDES JRX enabled mask: 0x0003
ad9088 spi1.0: Restoring ADC calibration data...
ad9088 spi1.0: Restoring SERDES RX calibration data...
ad9088 spi1.0: Restoring clock conditioning calibration data...
ad9088 spi1.0: Calibration data restored successfully

Best Practices

  1. Verify Saved Data: Always verify the saved file can be restored before relying on it in production

  2. Temperature Considerations: Calibration data is temperature-dependent:

    • Save calibration at operating temperature

    • Re-calibrate if temperature changes significantly

    • Consider separate calibration files for different temperature ranges

  3. Version Control: Track calibration data with device information:

    $
    
    echo "Chip ID: $(dmesg | grep AD9088 | grep 'Chip ID')" > /lib/firmware/ad9088_cal.txt
    
    $
    
    echo "Date: $(date)" >> /lib/firmware/ad9088_cal.txt
    
    $
    
    echo "Config: $(dmesg | grep 'is_8t8r')" >> /lib/firmware/ad9088_cal.txt
    

Security Considerations

  • The calibration_data sysfs attribute has 0600 permissions (root read/write only)

  • Calibration data is device-specific and cannot be shared between different chip instances

  • CRC32 validation ensures data integrity

  • No sensitive information is stored in calibration data

Source Code

Calibration-related source files: