iio_attr
iio_attr - list IIO devices, and read/write device attributes
SYNOPSIS
DESCRIPTION
iio_attr is a utility for displaying information about local or remote IIO devices. By providing an optional value, iio_attr will attempt to write the new value to the attribute.
COMMANDS
The iio_attr utility has a few main options, which control what the main utility of the application is.
- -d, –device-attr
Read and Write IIO device attributes
- -c –channel-attr
Read and Write IIO channel attributes
- -B –buffer-attr
Read and Write IIO Buffer attributes
- -C –context-attr
Read and Write IIO Context attributes
- -D –debug-attr
Read and Write IIO Debug attributes
- -E –event-attr
Read and Write IIO device event attributes
- -e –channel-event-attr
Read and Write IIO channel event attributes
- -h, –help
Tells iio_attr to display some help, and then quit.
- -V, –version
Prints the version information for this particular copy of iio_attr and the version of the libiio library it is using. This is useful for knowing if the version of the library and iio_attr on your system are up to date. This is also useful when reporting bugs.
- -S, –scan [backends]
Scan for available IIO contexts, optional arg of specific backend(s) ‘ip’, ‘usb’ or ‘ip,usb’. Specific options for USB include Vendor ID, Product ID to limit scanning to specific devices ‘usb=0456:b673’. vid,pid are hexadecimal numbers (no prefix needed), “*” (match any for pid only) If no argument is given, it checks all that are available.
OPTIONS
- -u, –uri
The Uniform Resource Identifier (uri) for connecting to devices, can be one of:
- ip:[address]
network address, either numeric (192.168.0.1) or network hostname
- ip:
blank, if compiled with zeroconf support, will find an IIO device on network
- usb:[device:port:instance]
normally returned from iio_attr -S
- serial:[port],[baud],[settings]
which are controlled, and need to match the iiod (or tinyiiod) on the other end of the serial port.
- [port]
is something like ‘/dev/ttyUSB0’ on Linux, and ‘COM4’ on Windows.
- [baud]
is normally one of 110, 300, 600, 1200, 2400, 4800, 9600, 14400, 19200, 38400, 57600, 115200 [default], 128000 or 256000, but can vary system to system.
- [settings]
would normally be configured as ‘8n1’ this is controlled by:
- data_bits:
(5, 6, 7, 8 [default], or 9)
- parity_bits:
(‘n’ none [default], ‘o’ odd, ‘e’ even, ‘m’ mark, or ‘s’ space)
- stop_bits:
(1 [default, or 2)
- flow_control:
(‘0’ none [default], ‘x’ Xon Xoff, ‘r’ RTSCTS, or ‘d’ DTRDSR)
- local:
with no address part.
- -T, –timeout <arg>
Context timeout in milliseconds. 0 = use backend default, -1 = wait forever, ‘nb’ or ‘nonblocking’ = non-blocking mode. Default is 0.
- -w, –write-only
Do not readback on Writes
- -i, –input-channel
Filters channels by input channels only
- -o, –output-channel
Filters channels by output channels only
- -s, –scan-channel
Filters channels by scan channels only
- -I, –ignore-case
When pattern matching devices, channels or attributes, ignore case
- -g, –generate-code <arg>
Generate small C or python snippets that emulate what you are doing on the command line. Argument is a file name ‘foo.c’ or ‘foo.py’
- -b, –buffer-index <arg>
When reading or writing buffer attributes (-B), select the buffer at this index. When not specified, -B shows attribute counts for all buffers on the device.
- -f, –input-file
Treat the trailing [value] argument as a path to a file. The file’s raw bytes are written to the attribute via the _raw API variant, instead of writing [value] as a string. Cannot be combined with -C or –generate-code, and is rejected when used with wildcard matches. A short write (fewer bytes accepted than supplied) is reported as a WARNING on stderr.
RETURN VALUE
If the specified device is not found, a non-zero exit code is returned.
SEE ALSO
iio_attr(1), iio_info(1), iio_rwdev(1), iio_reg(1), libiio(3)
libiio home page: https://wiki.analog.com/resources/tools-software/linux-software/libiio
libiio code: https://github.com/analogdevicesinc/libiio
Doxygen for libiio https://developer.analog.com/docs/libiio/
BUGS
All bugs are tracked at: https://github.com/analogdevicesinc/libiio/issues