Command line interface
The Doctools bundles a command line interface called adoc meant to ease both
continuous integration and local builds of the documentation.
Below, each command is briefly described, and it is worth noting that every
command supports the --help option for quick lookup.
See MCP integration to learn how to integrate with your favorite AI coding harness.
Serve
Watches the docs and source code to rebuild it on edit.
Similar to mkdocs serve, webpack serve, npm run start, hugo server,
and so on.
The webpage pools timestamp changes and commands on the .dev-pool file.
To launch a watched instance, do:
~$
cd /path/to/docs
/path/to/docs$
adoc serve
Where /path/to/docs is the path to the folder containing the Sphinx Makefile.
To also watch changes made to theme itself, use the --dev option, just make
sure to have Doctools as Development install.
For PDF output, do:
/path/to/docs$
adoc serve --builder pdf
Make sure to use an PDF viewer that watches the file timestamp and automatically reloads, such as Gnome PDF (Evince).
Tip
The PDF’s table of contents depth is set by the top index page’s
maxdepth property of the toctree.
All options can be listed with:
~$
adoc serve --help
With the optional adi-doctools['gui'] installed, use --gui to launch a
full web editor see GUI support.
To how to integrate with your IDE, please see VScode/VScodium support and Neovim support.
Sparse builds
Inspired on git sparse clones, it is possible to build only some parts of the documentation, for example:
# Include only learning/**/* and solutions/**/*
~$
adoc serve --sparse learning solutions
This is a critical feature to build large docs, ensuring snappy live reloads.
How does it even work?
It sets up multiple Sphinx configurations:
interref_repos: [..., <repo>]: Add current repository tointersphinxcross-references.intersphinx_disabled_reftypes: ['']: Resolve any local reference as cross-reference, if not found locally.exclude_patterns: [...]: Exclude all files masked by--sparse, using known patterns.suppress_warnings: [..., 'toc.excluded', 'toc.empty_glob']: Suppress some toctree warnings caused by the mask.
The result is: the exclude list excludes files from being read, and if the built pages have local references and they are not found, they are linked to the remote inventory ./objects.inv, finally, the suppress warning list drops the warnings related to the excluded files in the table of contents.
Git LFS integration
Serve detects if a repository uses Git Large File Storage to fetch (smudge) the watched binaries on demand.
This enables users to clone a repo with git lfs install --skip-smudge
and only fetch, on demand, the binary resources they are working on,
significantly reducing clone time and bandwidth usage.
Caution
GIT_LFS_SKIP_SMUDGE=1 and --skip-smudge are not identical!
# Still fetches with either set.
$
git lfs pull -I pointer_file
# Only fetches with --skip-smudge, skipped with GIT_LFS_SKIP_SMUDGE=1
$
git lfs smudge < pointer_file > /tmp/file.png
The per-file fetch is triggered by a GET request, such as when opening the local server page in a browser, or by touching the watched source file.
The HTML GET request triggers a fetch for all Git LFS rules on the .gitattributes file, while a “touch” only works on file types that are also watched by the server.
If neither the GET request nor the touch file to fetch is suitable, it is possible to pull the file directly with:
git lfs pull public -I file_basename
Be mindful of the file_basename, e.g. my_image.jpg,
full paths like path/to/my_image.jpg will silently fail.
How can I rebuild the whole documentation within Serve?
Run make clean in another tab, it will trigger a full rebuild.
Do not do make clean html since it will generate a build without the
proper Serve environment and live reload won’t work properly.
Why is the output missing styling (CSS stylesheet)?
You probably did a Development install without Install the web compiler
and you are building directly (make html) instead of using Serve.
If you don’t want to install npm, use Serve and accept the prompt to
fetch the pre-built web-scripts from the latest release.
Why is the Python source code of this repo not watched?
Since a Python scripts change would affect rebuilding the whole documentation,
those files are not watched by design even with the --dev option.
Extensions at the doc itself are, however.
Alternatively, touch the source doc of the open page to rebuild only it with the edited Python code.
Search docs
Search Sphinx documentations. Works by fetching the searchindex.json and
objects.inv Uses the same search algorithm as Sphinx’s JavaScript search.
For example:
~$
adoc search ad9084 profile
[1] [documentation] AD9084
https://developer.analog.com/docs/.../ad9084/index.html
:external+documentation:ref:`ad9084 iio-oscilloscope` ...
AD9084 Capture Window Main receivers are handled by the axi-ad9081-rx-hpc
IIO device, The number of channels depend on the JESD mode (M) p...
[2] [scopy] AD9084
https://developer.analog.com/docs/scopy/plugins/ad9084/ad9084.html
:external+scopy:ref:`ad9084` :external+scopy:doc:`plugins/ad9084/ad9084`
AD9084 Overview The AD9084 instrument for Scopy enables integration
and control of the Apollo MxFE platform within the Scopy soft...
More examples:
~$
adoc search --repo documentation -- user guide
~$
adoc search --repo documentation,hdl,no-OS -- axi
~$
adoc search --url https://developer.analog.com/docs/hdl/2023_R2 -- ad4630
~$
adoc search --repo hdl --limit 10 -- axi
Fetch source
For a search, you can chain the adoc search --fetch command, for example:
~$
adoc search --fetch 1
Fetching source for: [2] EVAL-AD4060/AD4062-ARDZ
Repository: documentation
Document: solutions/reference-designs/ad4062-ardz/index
Source URL: https://.../reference-designs/ad4062-ardz/index.rst
.. collection:: EVAL-AD4060/AD4062-ARDZ
:subtitle: Evaluating the AD4060/AD4062 Compact, Low Power, 12-Bit/16-Bit, 2 MSPS Easy Drive SAR ADCs
:image: eval-angle.png
:label: eval user-guide
Search dokuwiki
As a transition tool, it is also possible to search the DokuWiki (https://wiki.analog.com):
~$
adoc search-wiki ad9084 profile
Usage is identical, but the fetch output is either DokuWiki markup or html.
Custom Doc
Generates custom documents with filtered content from all documentations of the watched repositories (see adi_doctools/lut.py).
For PDF output, LaTeX is used, please read PDF LaTeX support to how to setup.
To quick start, run the tool twice in an empty directory.
~$
cd /tmp/my_doc
/tmp/my_doc$
adoc custom-doc
Configuration file doc.yml not found, created template at:
/tmp/my_doc/doc.yml
Update it with the desired sources and rerun the tool.
/tmp/my_doc$
adoc custom-doc --builder pdf
[ build output ]
The doc.yml file is a concise human-readable markup file to set the desired content and some other options. Running the tool in a directory without the doc.yml will instantiate a template and return. If the necessary repositories are not found, the tool will clone for you.
In general, you can first clone and checkout your current work and then run the tool, to build the doc with your own changes.
Some documentations depend on auto generated sections and extra features, use
the --extra option to enable those; it considers that the environment has all
the tools needed, for example, vivado is accessible for the HDL documentation.
See adi_doctools/cli/custom_doc.py to understand how the extra steps are
included, but in summary, they are just a sequence of bash commands wrapped on python.
For all options, do:
~$
adoc custom-doc --help
Here is a minimal doc.yml:
project: Custom user guide
description: Subtitle of the user guide
include:
- documentation/software/libiio/cli.rst
custom:
- custom-pages/index.rst
entry-point:
- caption: My custom index
files:
- custom-pages/index.rst
config:
documentation:
branch: "my-branch"
extensions:
- sphinx.ext.duration
The include option contains the list of files to include in the custom
document, with the first level of the path the label (normally the repository
name).
During generation, the tool will resolve the hierarchy of the included docs, adding pages until the repository top-level page is reached. This may result in unwanted content being added and empty “category” sections.
To resolve that, it is possible to create custom top-level toctrees with the
entry-point option.
In summary, this:
entry-point:
- caption: HDL design
files:
- some/custom/intro.rst
- hdl/some/project.rst
Resolves at index.rst into:
.. toctree::
:caption: HDL design
some/custom/intro
hdl/some/project
Additional configuration can be added to the config option:
repository: Sets the repository to clone, if unset, is inferred as the label name. Useful when using the same repository multiple times for different branches.branch: Clone the repository from a specific branch, overwrite “main”. If the repository is already present, this option has no effect.extra: Do steps that require extra software, for example, some vendor SDK.
The option extensions allow appending extra Sphinx extensions, beyond the
automatically imported from the sourced documentations.
Generate the doc.yml from a collection
A collection directive describes which pages of which repositories belong together, and can be used to generate the doc.yml:
~$
cd /tmp/my_doc
/tmp/my_doc$
adoc custom-doc ~/documentation/docs/solutions/reference-designs/ad4052-ardz/index.rst
Generated doc.yml at /tmp/my_doc/doc.yml from ~/documentation/docs/solutions/reference-designs/ad4052-ardz/index.rst
[ build output ]
The page can also be an url:
~$
adoc custom-doc https://developer.analog.com/docs/documentation/solutions/reference-designs/ad4052-ardz/index.html
Just like Serve, Custom doc also has Git LFS integration. The current limitation is that only copied images (from the sphinx’s “copying images…” step) are looked for lfs pointers, so artifacts from other steps are missed, such as from the download directive.
Working with multiple docs
Suppose you edited and tested multiple docs together, it could be helpful to try a local inventory file first, to check references before publication.
Having this in mind, if you build the edited documentation first, and then execute
custom-doc, it will consider the local inventory objects.inv also.
Here is a example of auto-resolved intersphinx_mapping by custom-doc, at the
_build/conf.py:
# -- External docs configuration ----------------------------------------------
intersphinx_mapping = {
# Docs locally edited and referenced
'hdl':
('https://developer.analog.com/docs/hdl',
('/path/to/my_project/hdl/docs/_build/html/objects.inv', None)),
'documentation':
('https://developer.analog.com/docs/documentation',
('/path/to/my_project/documentation/docs/_build/html/objects.inv', None)),
# Doc not locally edited, but referenced
'scopy':
('https://developer.analog.com/docs/scopy', None),
}
Learn more about the core of this behavior at
sphinx.ext.intersphinx’s intersphinx_mapping.
For a single doc, without custom-doc, there is also interref_local described
at In-organization references doctools.
Aggregate
Tip
This feature is useful to batch build/test all tracked documentations.
Generates all documentations of the watched repositories (see adi_doctools/lut.py).
Two generation strategies are available:
monolithic: patches all docs together into a single monolithic output (default).
symbolic: generate each doc independently, just save them together (
--symbolic).
For the monolithic output, do:
/tmp/all-docs$
adoc aggregate
Some documentations depend on auto generated sections and extra features, use
the --extra option to enable those; it considers that the environment has all
the tools needed, for example, vivado is accessible for the HDL documentation.
See adi_doctools/cli/aggregate.py to understand how the extra steps are
included, but in summary, they are just a sequence of bash commands wrapped on python.
For all options, do:
~$
adoc aggregate --help