Skip to content

Uninstall CodeFusion Studio

Uninstall the extension from VS Code

  1. Select the Extensions icon from the activity bar.
  2. Find the CodeFusion Studio extension in the INSTALLED list.
  3. Click on the Manage (cog) icon on the right hand side.
  4. Select Uninstall.

CodeFusion Extension Uninstall CodeFusion Extension Uninstall

Note

Keyboard shortcut to extensions is Control + SHIFT + X (Windows/Linux) or Command + SHIFT + X (Mac).

Uninstall from file system

You can uninstall CodeFusion Studio using the Maintenance Tool.

  1. Navigate to the directory where CodeFusion Studio is installed.
    • The Windows default location is C:\analog\cfs\
    • The macOS or Linux default location is ~/analog/cfs/
  2. Open the folder for the version you want to uninstall.
  3. Launch the Maintenance Tool:
    • On Windows, double click MaintenanceTool.exe
    • On macOS, double click MaintenanceTool.app
    • On Ubuntu, double click MaintenanceTool
  4. Select Remove all components and follow the prompt to continueInstaller Setup
  5. Check that the correct directory is being removed and click Uninstall.Ready to Uninstall
  6. CodeFusion Studio will now be uninstalled.Uninstall In Progress
  7. When the process completes, close the uninstaller Completed Uninstallation

Uninstall packages

For CFS 2.0.0, SDKs, plugins, and data models are installed using the Package Manager. These packages are stored locally and are not removed when you uninstall CFS 2.0.0.

To fully reset your environment and remove cached packages, delete the following directory:

  • Linux: /home/<username>/.local/share/com.analog.cfs
  • macOS: /Users/<username>/Library/Preferences/com.analog.cfs
  • Windows: C:\Users\<username>\AppData\Local\com.analog.cfs

Command line uninstall

Use the following command to uninstall CodeFusion Studio from the default location:

  • Windows: C:\analog\cfs\2.0.0\MaintenanceTool.exe purge
  • Linux: ~/analog/cfs/2.0.0/MaintenanceTool purge
  • macOS: ~/analog/cfs/2.0.0/MaintenanceTool.app/Contents/MacOS/MaintenanceTool purge