Skip to content

Software requirements

Software dependencies

The CodeFusion Studio VS Code extension depends on:

Note

Older versions of VS Code (such as 1.98 and earlier) are not supported due to known layout issues in the System Planner > Pin Config canvas.

Host OS support

CodeFusion Studio and its extension are supported on the following host operating systems:

  • Windows 11 (64-bit)
  • macOS 15 and macOS 26 (ARM64)
  • Ubuntu 22.04 and 24.04 (64-bit)

Earlier or newer OS versions may work but are not officially supported.

Linux support

The CodeFusion Studio installer requires the following packages in order to run.

sudo apt install libfontconfig1 libdbus-1-3 libxcb-icccm4 libxcb-image0 libxcb-keysyms1 libxcb-render-util0 libxcb-shape0 libxcb-xinerama0 libxkbcommon-x11-0 libgl1

Note

These packages are included in default Ubuntu installations, but may need to be added to headless installations.

Windows support

The AI Tools (including the Embedded AI Tools panel and the cfsai command-line utility) require the Visual C++ Redistributable for Visual Studio 2015 to be installed.

Install this redistributable manually before running the AI Tools.