Core Dump Analysis Tool overview
The Core Dump Analysis Tool enables developers to inspect the state of Zephyr-based firmware for supported SoCs at the time of a crash. It supports post-mortem debugging using core dumps generated by Zephyr-based applications.
Supported processors
Core dump analysis supports Zephyr RTOS applications on the following SoCs:
- MAX32657
- MAX32690
Support extends to all processor cores included in these SoCs.
Platform support
On macOS, the GDB binary used for Core Dump Analysis is not Python-enabled by default. For setup instructions, see the Release Notes.