Debug a SHARC-FX application
Use this guide to connect, configure, and debug SHARC-FX processors in CodeFusion Studio. The SHARC-FX family includes both single-core DSPs (such as the ADSP-2183x series) and multicore SoCs (such as the ADSP-SC83x family) that combine a SHARC-FX DSP with an ARM Cortex-M33 core.
Most of the setup steps, including toolchain installation and ICE emulator configuration, apply to all SHARC-FX devices. For single-core DSPs, debugging is performed directly on the SHARC-FX core. For multicore SoCs, the debugging process requires starting the SHARC-FX core before attaching to the ARM core.
Windows only
The SHARC-FX toolchain and related workspace plugins are supported only on Windows.
Proceed only if you are using a Windows host system.
Before you start
- Install ADI ICE drivers.
Ensure the ICE-1000, ICE-1500, or ICE-2000 drivers are installed so CodeFusion Studio can communicate with your SHARC-FX target.
- If you selected ADI ICE Drivers (Requires Administrator) during CodeFusion Studio installation, you’re all set.
- If you skipped that option, see Install ICE drivers manually.
- Sign in to the Package Manager and install the required SHARC-FX toolchain.
Step 2 – Log in to access the SHARC-FX toolchain
Authentication is required to download the SHARC-FX toolchain.
- Follow the steps in Access restricted packages (using myAnalog login).
- Install the toolchain using one of the following methods:
- Command Palette: Open the Command Palette and run CFS: Install Required Packages. Find
xtensa_sharcfx_toolchain/15.4.0in the list and click to install. -
Command line: From
cfsutil, runcfsutil pkg install xtensa_sharcfx_toolchain/15.4.0
- Command Palette: Open the Command Palette and run CFS: Install Required Packages. Find
Create a SHARC-FX workspace
- Follow the steps in Create a new workspace to launch the Workspace Creation Wizard.
- Select a SHARC-FX device, such as the ADSP-SC835W SoC and corresponding ADSPSC835W-EV-SOM board.
- Choose a SHARC-FX workspace template, such as SHARC-FX Multi-Core with TFLM running on the ARM core.
- Follow the prompts to complete workspace setup.
Connect the ICE emulator
The ICE-1000, ICE-1500, or ICE-2000 emulators are required for JTAG debugging on all SHARC-FX projects.
Follow the recommended setup for your ICE emulator:
- Connect the emulator and board:
- Attach the main power/data cable from the ADSP-SC835W board to your computer.
- Attach the main USB cable from the ICE emulator to your computer.
- Connect the emulator ribbon cable (ICE-1000, ICE-1500, or ICE-2000) to the board’s JTAG header.
- Verify that both the board and emulator LEDs flash green, indicating that the hardware is powered and communication is established.
-
Open Windows → Device Manager and confirm that the emulator appears under CrossCore Tools:
-
By default, CodeFusion Studio templates use the ICE-2000 interface. If you are using a different model, update the
.vscode/settings.jsonfor each project accordingly:"cfs.openocd.interface": "interface/ice1000.cfg" -
If you are using and ICE-1000 and ICE-1500 emulator, the value of adapter speed in
.vscode/launch.jsonshould also be updated in the SHARC-FX project. For ICE-1000 and ICE-1500, the maximum speed is 5000:"openOCDLaunchCommands": ["adapter speed 5000"],
Note
For additional information on installing the emulator hardware and software on your PC, see the ICE-1000/ICE-2000 Emulator User’s Guide (PDF).
Build the projects
Run the CFS: build to create the build directory and generate the ELF files needed for debugging.
- Click the CFS icon
in the Activity Bar. - In the Actions view, select the appropriate build task for your project:
- Select Build (m33) and Build (sfx) for multicore SHARC-FX SoCs.
- Select Build (sfx) for single-core SHARC-FX SoCs.
Start debugging
The steps below apply to multicore SHARC-FX SoCs such as the ADSP-SC83x family. For ADSP-SC83x projects, debugging on the ARM core works only if the SHARC-FX core is started first, then the ARM debug session is started.
If you are using a single-core SHARC-FX DSP, start a standard debug session for the SHARC-FX project only.
To start debugging:
- Select the Run and Debug icon on the activity bar.
- Select the Debug with GDB and OpenOCD (sfx) from the dropdown menu.
- Click on the Start Debugging icon (green play button) to the left of your selection or press F5. This will load and run the preload application, which will configure clocks and DMC settings. The main application can then be loaded and run by clicking on the Reset device icon.
- When the SHARC-FX debug session starts and the core halts at
main(), leave it running. - Launch the ARM debug instance using the Debug with GDB and OpenOCD (ARM) debug configuration.
Note
During an active debug session, the ICE emulator LED changes to purple, indicating that it is connected and debugging.
Troubleshooting
| Error Message | Solution |
|---|---|
Failed to launch GDB: could not connect (error 138): The system tried to join a drive to a directory on a joined drive |
Start debugging with the SHARC-FX core first. |
Cannot find: "C:/analog/cfs/2.0.0/Tools/xtensa/RJ-2024.4/XtensaTools" |
Ensure you install the Xtensa toolchain package. |
OpenOCD: GDB Server Quit Unexpectedly. |
Update the .vscode/settings.json for each project with the correct ICE emulator model |