Zephyr RTOS projects
Modify west commands
CodeFusion Studio generates a default west build command for your current project (ex.: west build -b apard32690/max32690/m4).
While the default west build command covers most common build cases, there are situations where you need to pass additional parameters to west.
Examples of common cases where you want to alter the west build command include:
- Setting one-off KConfig parameters that you only want to use for one build:
-DCONFIG_FAULT_DUMP=1 - Associating an optional config overlay file with your build:
-DOVERLAY_CONFIG=my-overlay.conf - Specifying a 'shield' to use with your development board:
-DSHIELD=shield_name
There are two main ways you can customize the west build command in CodeFusion Studio:
- Modify the task associated with the 'build' action.
- Manually enter a west command using The CFS Terminal.
Example one
To perform a west build with additional OVERLAY_CONFIG parameters, tell the build system to include this config file in the build operation by passing the parameters on the CFS terminal as follows:
west build -p auto -b apard32690/max32690/m4 -- -DOVERLAY_CONFIG=my-overlay.conf
Example two
To debug an application and receive more details when hitting a fault handler, do a one-off build with the CONFIG_FAULT_DUMP KConfig flag set:
west build -p auto -b apard32690/max32690/m4 -- -DCONFIG_FAULT_DUMP=1
Note
The double dash -- in the west command line will pass any following arguments directly to CMake.
Add compiler arguments
To pass specific compiler switches to the build system, use zephyr_cc_option in CMakeLists.txt:
zephyr_cc_option(-fstack-usage)