Tasks to build, clean, flash and debug
After creating a workspace and configuring it, you can run various tasks to create, flash, clean, and run applications.
Access the tasks
Tasks can be accessed in the following ways:
- Command palette: Open the command palette (
Ctrl+Shift+PorCmd+Shift+Pon macOS) from the Manage gear icon and enter the task name. - Actions view: Click the CFS icon
in the Activity Bar, then choose a task from the Actions view. You can also create new custom tasks by clicking Copy and Edit 
next to each task. - Status Bar: Click a relevant icon (build, flash, erase) on the left side of the Status Bar.
- From the menu: Go to Terminal > Run Build Task, then select the desired task.
Note
All tasks operate in the same way independent of the mechanism used to invoke them.
Tasks
CFS: build
The CFS: build task compiles the code using make. Options are passed into the make file on the command line based on the project's settings.json file. It creates the ./build directory, which contains the output binary and all intermediary object files.
The build configuration variables used by the makefiles are set during workspace creation, or in the workspace, user or system settings.
Note
Shortcut: Ctrl + Shift + B (Windows/Linux) or Command + Shift + B (Mac).
The build task is also available with shortcuts on the left-hand side of the status bar.

CFS: clean
The CFS: clean task cleans the build output, removing the ./build directory and all of its contents.
CFS: clean-periph
The CFS: clear-periph tasks runs CFS: clean as well as removes the build output for the MSDK's peripheral drivers. Use CFS: clean-periph to recompile the peripheral drivers from source on the next build.
CFS: flash
The CFS: flash task first runs the CFS: build task. Then, it flashes the output binary to the microcontroller. It uses the GDB load and compare-sections commands, and launches an OpenOCD internally using a pipe connection. This halts the flashed program until the microcontroller is reset, power cycled, or a debugger is connected. A debugger must be connected correctly to use this task. Refer to the data sheet of your microcontroller's evaluation board for instructions.
CFS: flash and run
The CFS: flash and run task runs the CFS: flash task and resumes execution of the program after flashing is complete.
CFS: erase flash
The CFS: erase flash task erases all of the application code in the flash memory bank. After running this task, the target microcontroller is effectively blank. This is useful for recovering from low power (LP) lockouts, bad firmware, or other issues.
CFS: debug
The CFS: debug task will launch the previous debug session. This may run the CFS: flash command before running the application and halting at the breakpoint at main(). The executable file will need to be built using the CFS: build command before debugging. Care should be made to ensure the executable is up to date before debugging.
Using the activity view you can select a debug session to launch. See Debugging an application for more information.
Create custom tasks
To create a custom build or flash task, do one of the following:
- Click the dropdown arrow in the Terminal panel and select Configure Tasks. Then choose a task from the list to copy.
- In the Actions view, click Copy and Edit

next to the task you want to duplicate.
This opens your project's .vscode/tasks.json file and adds a copy of the selected task. You can now edit the copy without affecting the original.
The new task also appears as a separate entry in the Actions view, with a label that starts with CFS: (for example, CFS: build).
Tip
To personalize your task, append a description to the label in tasks.json. For example: "label": "CFS: build MAX32690-debug"
Modify build tasks
To modify a custom build or flash task, do one of the following:
- Click the dropdown arrow in the Terminal panel and select Configure Tasks. Then choose the task your previously created from the list.
- In the Actions view, click Edit

next to your custom task.
The .vscode/tasks.json file opens in your editor. You can update the task directly in the file.
For more information on modifying build tasks, see Custom tasks