Catalog Manager
The Catalog Manager is a background service in CodeFusion Studio that retrieves and maintains the SoC catalog. This catalog provides the latest metadata for supported System-on-Chip (SoC) devices, ensuring access to up-to-date information on documentation, cores, boards, and packages.
Settings
During installation, a backup copy of the catalog is stored in the <install_dir>/Data/Soc/catalog.zip directory.
The working copy of the catalog manager is stored at: <${userHome}>/cfs/<cfs_version_number>/.catalog.
The Catalog Manager regularly checks for updates to the SoC catalog. If using Offline Mode, the most recently cached catalog data is used.
CFS Settings
Note
For details on accessing CFS settings, see CFS Settings.
The Catalog Manager has the following user and workspace CFS settings:
- Offline Mode (
cfs.catalogManager.checkForUpdates) – Use to work with a local cached catalog if an internet connection is unavailable. - Catalog Location (
cfs.catalogManager.catalogLocation) – Specifies the directory where the working copy of the catalog manager is stored. This location contains temporary files that store processed SoC data. - Catalog URL (
cfs.catalogManager.url) – Specifies the cloud service used to fetch updates.
Troubleshooting
Refer to the following table for Catalog Manager errors and their resolutions.
| Error Message | Possible Cause | Resolution |
|---|---|---|
| Catalog Manager failed to initialize with error: [error message] | There is an issue with the catalog zip, or the CFS settings need to be reviewed. | Verify that <install_dir>/Data/Soc/catalog.zip exists. Check if any cfs.catalogManager settings have changed, including catalogLocation and url. If needed, restore correct settings and restart CodeFusion Studio. |
| Failed to get catalog: [error details] | The Catalog Manager was unable to fetch the catalog from the cloud. | Check your internet connection. If the cloud service is unavailable, enable Offline Mode. If needed delete the .catalog folder and restart CodeFusion Studio. |