Install Olimex USB ARM JTAG Drivers for RISC-V Debugging
The Olimex ARM-USB-OCD-H debugger is required to debug the RISC-V core on supported MAX32xxx and MAX78xxx devices. The Olimex drivers are not provided directly by CodeFusion Studio so need to be installed manually if RISC-V debugging is required.
Download and installation instructions can be found in chapter 3 of the Olimex ARM-USB-OCD-h User Manual
Linux configuration
On Linux the user may need to be added to the dialout group in order to use the Olimex Debugger.
sudo usermod -aG dialout <username>