Debug a multi core application
CodeFusion Studio provides debugging for supported microcontrollers with multiple cores.
The multi-core architecture of the MAX32xxx and MAX78xxx microcontrollers requires secondary images contained within the image for the primary core.
This means only a single image is required to boot and run a multi-core microcontroller.
The secondary core is enabled with a code sequence on the primary core. Debugging the secondary core is available after MXC_SYS_RISCVRun() has been called on the primary core.
Note
Not all of the dual core evaluation boards have external debug ports for the secondary core. Care should be taken when selecting a board to work with.
See Supported processors for a full list of supported processors.
Create a multi-core workspace
To get started, you need to create a multi-core workspace. There are two options:
- Create a multi-core workspace using the Workspace Creation Wizard
- Create a multi-core workspace by combining two SDK examples
Option 1: Create a multi-core workspace using the Workspace Creation wizard
- Click the CodeFusion Studio icon
in the VS Code activity bar. - Click New Workspace.
- Select the MAX78002 processor and EvKIT_V1 board.
- Choose Select a workspace template and select the MSDK multi-core example.
- Click Continue.
- Enter a name for your workspace and click Create Workspace.
Option 2: Create a multi-core workspace by combining SDK examples
The MAX78002 RV_ARM_Loader example is located within the CodeFusion Studio installation at <CodeFusion Studio Install>/SDK/MAX/Examples/MAX78002/RV_ARM_Loader. This example uses the Arm processor to load and prepare the RISC-V processor to run a chosen program.
Note
By default, the example runs the MAX78002 Hello_World example on the RISC-V processor, found at <CodeFusion Studio Install>/SDK/MAX/Examples/MAX78002/Hello_World. To run a different program on the RISC-V processor, change the RISCV_APP variable in RV_ARM_LOADER/project.mk to point to the root directory of the program to build and run:
project.mk
# This file can be used to set build configuration
# variables. These variables are defined in a file called
# "Makefile" that is located next to this one.
# For instructions on how to use this system, see
# https://analogdevicesinc.github.io/msdk/USERGUIDE/#build-system
# **********************************************************
# Enable the RISC-V loader
RISCV_LOAD = 1
# The RISCV application can be changed.
# It defaults to Hello_World
RISCV_APP=../Hello_World
-
Create a new directory, such as
MAX78002_Multicore, outside of the SDK examples folder. -
Copy the
MAX78002Hello_Worldexample (or the example you'd like to run on the RISC-V processor) and theMAX78002RV_ARM_Loaderexample into theMAX78002_Multicoredirectory.Note
If the
Hello_Worldproject isn't located at../Hello_Worldrelative toRV_ARM_Loader, or if you are using a different project, you will need to update theRISCV_APPpath inRV_ARM_Loader/project.mk. -
Click File > Open Folder to open the copied
RV_ARM_Loaderfolder as single-folder workspace. -
Click File > Add Folder to Workspace to add the copied
Hello_Worldfolder.Note
Convert the projects to CodeFusion Studio workspaces if required. See Open and Migrate Example for more info.
Build the projects
Run the CFS: build to create the build directory and generate the ELF files needed for debugging.
- Click the CFS icon
in the Activity Bar. - Select Build (m4) or Build (RV_ARM_Loader) in the Actions view.
This action creates the following files:
build/m4.elforbuild/RV_ARM_Loader.elfbuild/buildrv/riscv.elf
Debug settings
- Select the Run and Debug icon on the activity bar.
- Select the CFS: Debug with GDB and OpenOCD (Arm Embedded) from the dropdown menu.
- Click on the Start Debugging icon (green play button) to the left of your selection or press F5.
-
Select configuration or image files if prompted.
Note
If prompted to specify the Arm ELF binary, the path depends on your project layout:
-
If you are using the
m4core directory from the template use:
<workspace-folder>/m4/build/m4.elf -
If you are using the
RV_ARM_Loaderexample use:
<workspace-folder>/RV_ARM_Loader/build/RV_ARM_Loader.elf.
-
-
When the Arm debug session reaches the breakpoint in the main.c code, press Continue on the debugging tool bar or F5.
- Confirm RISC-V is running by observing LED0 blinking, or pause the Arm core to check it has passed the call to
MXC_SYS_RISCVRun(); - Launch the RISC-V debug instance using the CFS: Debug with GDB and OpenOCD (RISC-V) debug configuration.
-
Select configuration/image files if prompted.
Note
If prompted to specify the RISC-V ELF binary, the path depends on your project layout:
-
If you are using the
m4core directory from the template use:
<workspace-folder>/m4/build/buildrv/riscv.elf -
If you are using the
RV_ARM_Loaderexample use:
<workspace-folder>/RV_ARM_Loader/build/buildrv/riscv.elf
-
Control the session
The Call Stack can be used to navigate between each debug instance. This provides quick access to the debugging taking place on each processor.