Supported Processors
CodeFusion Studio currently supports the following processors in the following configurations:
| Processor | MSDK | Zephyr | Config Tools | TESA |
|---|---|---|---|---|
| MAX32650 | Yes | Yes | No | Yes1 |
| MAX32655 | Yes | Yes | Yes | Partial2 |
| MAX32660 | Yes | Yes | No | No |
| MAX32662 | Yes | Yes | No | Partial2 |
| MAX32666 | No | Yes | No | No |
| MAX32670 | Yes | Yes | No | Yes1 |
| MAX32672 | Yes | Yes | No | Partial2 |
| MAX32675C | Yes | Yes | No | No |
| MAX32690 | Yes | Yes | Yes | Yes1 |
| MAX78000 | Yes | Yes | No | Partial2 |
| MAX78002 | Yes | Yes | No | No |