Purpose
Embedded software engineering is becoming an increasingly complex challenge. As the industry shifts toward heterogeneous multi-core systems, engineers must configure and debug multiple processing architectures while maintaining efficiency. At the same time, shrinking development resources and tighter time-to-market pressures exacerbate these challenges.
Engineers are expected to deal with this complexity with tools, middleware, and SDKs designed for a single-core, single-architecture world. Those tools are often proprietary, single-vendor solutions that may become obsolete. Code generated from these tools is typically inflexible, with limited usefulness in the real world.
Why CodeFusion Studio
The award-winning CodeFusion Studio (CFS) is an embedded software development platform built on Microsoft’s open-source Visual Studio Code, designed to simplify multi-core, multi-architecture embedded development.
CFS solves the challenges of modern embedded engineering with an open-source toolset built for multi-core systems. It enables heterogeneous multi-core application development, system-wide resource management, debugging, and optimization — all without the restrictions of activation servers, licensing fees, or vendor lock-in.
Open source
CFS adheres to an Open Source First design principle. It provides embedded engineers with robust, extensible tools that they own, designed for long-term use and customization.
-
Apache-licensed tooling for full ownership of the software development pipeline
-
Permissively-licensed tools for customization
-
Open-source toolchains and critical software components
-
Integration with Zephyr, an open-source operating system
System visibility
CFS provides better system visibility into complex systems.
-
System Planner dashboard: Use the intuitive graphical interface to allocate memory partitions, peripherals, clocks, and pins per core, reducing conflicts in multi-core SoCs.
-
ELF File Explorer: Quickly parse, analyze, and debug compiled binaries, minimizing time spent on debugging and performance profiling.
-
Heterogenous multi-core debugging: Debug multiple cores in a single unified environment, eliminating the need for multiple IDEs. One IDE, one debug session, one hardware debugger.
-
Integrated register viewer: Eliminates the need for repetitive datasheet lookups by providing a graphical representation of configuration registers used in the system configuration.
Flexibility
CFS also provides flexibility by consolidating technical information in a single data source, for easy integration into custom tooling and modern automated workflows.
-
SoC (System on Chip) Data Model: Provides detailed technical information, including the relationships between config choices and registers, memory layouts, and pin multiplexing. The SoC data model syncs with the Catalog Manager, ensuring engineers always have access to the latest hardware data without needing manual updates.
-
Command-Line First: Ensures critical actions run on the CLI, enabling compatibility with modern CI pipelines, and improving test, build, and deployment processes.
-
Graphical Resource Allocation: Provides the flexibility to allocate and configure memory and peripherals across cores using the System Planner Configuration Tools dashboard, managing SoC resource constraints in one place.
-
Plugin-Based Project Creation: A flexible, plugin-driven system that supports multiple RTOS and firmware platforms. Developers can add custom plugins to generate configuration and project files tailored to specific development standards.
-
Open Interfaces for Code Generation: Plugins capture GUI-defined settings at various stages of the development process, generating project and configuration files that fit internal HALs, middleware, and coding standards.
Goals
CFS aims to bring embedded software into the modern, heterogeneous world. It enables repeatable, testable, and maintainable development pipelines that customers fully own. It creates a window into complex, opaque systems, offering a clearer view of resource allocation and system performance. Above all, it aims to provide engineers with the long-term flexibility and adaptability needed to develop solutions that last as long as the hardware they support.