Uninstall CodeFusion Studio
Uninstall the extension from VS Code
- Select the Extensions icon from the activity bar.
- Find the CodeFusion Studio extension in the INSTALLED list.
- Click on the Manage (cog) icon on the right hand side.
- Select Uninstall.
Note
Keyboard shortcut to extensions is Control + SHIFT + X (Windows/Linux) or Command + SHIFT + X (Mac).
Uninstall from file system on Windows
- Navigate to the directory where CodeFusion Studio is installed.
- Locate the MaintenanceTool.exe application and double click on it.

- After the MaintenanceTool.exe application launches, select Remove all components from the setup menu.

- Click Next to continue.
- Confirm that the correct directory is being removed and click Uninstall.

- CodeFusion Studio will now be uninstalled.

- After the uninstallation completes, you may close the installer by clicking Finish.

Remove the file system on Linux or Mac
The CodeFusion Studio directory can be deleted directly from the filesystem without needing to run an uninstall utility.