Tasks to build, clean, flash and debug
After creating a project and configuring the workspace, you can run various tasks to create, flash, clean, and run applications.
Access the tasks
Tasks can be accessed in the following ways:
- Open the Terminal menu and select run build task, and select the task.
- Open the command palette and enter the task name.
- Click on the CodeFusion Studio icon on the activity bar and then select a task from the Actions view (3 in the diagram below).
- Click on the icon in the left side of the status bar (5 in the diagram below).
- Select the desired build task:
Note
All tasks operate in the same way independent of the mechanism used to invoke them.
Tasks
CFS: build
The CFS: build task compiles the code using make. Options are passed into the make file on the command line based on the project's settings.json file. It creates the ./build directory, which contains the output binary and all intermediary object files.
The build configuration variables used by the makefiles are set during project creation or in the workspace, user or system settings.
Note
Shortcut: Ctrl + Shift + B (Windows/Linux) or Command + Shift + B (Mac).
The build task is also available with shortcuts on the left-hand side of the status bar.

CFS: clean
The CFS: clean task cleans the build output, removing the ./build directory and all of its contents.
CFS: clean-periph
The CFS: clear-periph tasks runs CFS: clean as well as removes the build output for the MSDK's peripheral drivers. Use CFS: clean-periph to recompile the peripheral drivers from source on the next build.
CFS: flash
The CFS: flash task first runs the CFS: build task. Then, it flashes the output binary to the microcontroller. It uses the GDB load and compare-sections commands, and launches an OpenOCD internally using a pipe connection. This halts the flashed program until the microcontroller is reset, power cycled, or a debugger is connected. A debugger must be connected correctly to use this task. Refer to the data sheet of your microcontroller's evaluation board for instructions.
CFS: flash and run
The CFS: flash and run task runs the CFS: flash task and resumes execution of the program after flashing is complete.
CFS: erase flash
The CFS: erase flash task erases all of the application code in the flash memory bank. After running this task, the target microcontroller is effectively blank. This is useful for recovering from low power (LP) lockouts, bad firmware, or other issues.
CFS: debug
The CFS: debug task will launch the previous debug session. This may run the CFS: flash command before running the applicationand halting at the breapoint at main(). The executable file will need to be built using the CFS: build command before debugging. Care should be made to ensure the executable is up to date before debugging.
Using the activity view you can select a debug session to launch. See Debugging an application for more information.
Modify build tasks
To modify the default build and flash tasks, click the Terminal menu and select Configure Tasks.... Select the task you wish to modify. A copy of the task will be added to your project's .vscode/tasks.json file, where it can be adjusted to suit your application's needs.
For information on modifying build tasks, see https://code.visualstudio.com/docs/editor/tasks#_custom-tasks