CFS Settings
Overview
CodeFusion Studio provides additional settings within VS Code.
Settings are saved at either the User, Workspace, or Folder level depending on the number of projects within a configured workspace, and are used hierarchically: Folder > Workspace > User.
- User settings can be modified from the
File > Preferences > Settingsmenu. - Workspace settings can be modified from the
File > Preferences > Settingsmenu or by editing the.vscode/settings.jsonin your workspace. - Folder settings can be modified by editing the
.vscode/settings.jsonin your sub directory. Workspace settings are created when a project is created and will have values related to that project. User settings have the default values below:
| ID | Description | User Default Value |
|---|---|---|
| cfs.cmsis.pack | Absolute path to the CMSIS pack | null |
| cfs.cmsis.root | Path to the root CMSIS pack directory | ${userHome}/AppData/Local/Analog/Packs |
| cfs.cmsis.svdFile | Absolute path to the .svd file. | |
| cfs.configureWorkspace | Whether this workspace should be configured as an CodeFusion IDE project. | No |
| cfs.debugger.SWD | Select the debugger to use. | MAX32625PICO |
| cfs.debugPath | Path to the directory containing the ELF binary to debug | null |
| cfs.openocd.interface | Absolute path to the OpenOCD interface script | null |
| cfs.openocd.riscvInterface | Absolute path to the OpenOCD interface script for RISCV core | null |
| cfs.openocd.path | Path to openocd | ${config:cfs.sdk.path}/OpenOCD |
| cfs.openocd.target | Absolute path to the OpenOCD target / board script | null |
| cfs.openocd.riscvTarget | Absolute path to the OpenOCD target / board script for RISCV core | null |
| cfs.programFile | ELF binary to debug | null |
| cfs.riscvProgramFile | ELF binary to debug | null |
| cfs.project.board | Target Board Support Package (BSP) | EvKit_V1 |
| cfs.project.name | Project name | ${workspaceFolderBasename} |
| cfs.project.target | Target processor | MAX78000 |
| cfs.sdk.path | Absolute path to your CodeFusion IDE | null |
| cfs.toolchain.armAArch32GCC.path | Path to the arm-none-eabi GCC toolchain | ${config:cfs.sdk.path}/Tools/gcc/arm-none-eabi |
| cfs.toolchain.riscVGCC.path | Path to the RISCV GCC toolchain | ${config:cfs.sdk.path}/Tools/gcc/riscv-none-elf |
| cfs.toolchain.selectedToolchain | The toolchain to build the current project with | arm-none-eabi |
| cfs.openHomePageAtStartup | Launch the CFS home page when a CFS project is opened | Yes |