Skip to content

Software requirements

Software dependencies

Tools VS Code extensions depend on:

Host OS support

CodeFusion Studio and extensions are supported on the following host operating systems:

  • Windows 10 or 11 (64-bit)
  • macOS (ARM64)
  • Ubuntu 22.04 and later (64-bit)

Linux support

The CodeFusion Studio installer requires the following packages in order to run.

sudo apt install libfontconfig1 libdbus-1-3 libxcb-icccm4 libxcb-image0 libxcb-keysyms1 libxcb-render-util0 libxcb-shape0 libxcb-xinerama0 libxkbcommon-x11-0 libgl1

Note

These packages are included in default Ubuntu installations, but may need to be added to headless installations.