Supported Processors
CodeFusion Studio currently supports the following processors in the following configurations:
| Processor | MSDK | Zephyr | Pin Config | Clock Config |
|---|---|---|---|---|
| MAX32655 | Yes | - | - | - |
| MAX32662 | Yes | - | - | - |
| MAX32670 | Yes | - | - | - |
| MAX32672 | Yes | - | - | - |
| MAX32675 | Yes | - | - | - |
| MAX32690 | Yes | Yes | Yes | Yes |
| MAX78000 | Yes | - | - | - |
| MAX78002 | Yes | - | Yes | - |